STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

[STM32F4] How to download and unzip selected files?

I want to install STM32Cube MCU Package for STM32F4 Series.​When I install ver 1.26.2, "stm32cube_fw_f4_v1260.zip" is installed and unzipped at first.In "stm32cube_fw_f4_v1260.zip", the folder "STM32Cube_FW_F4_V1.26.0" is included.Then, "stm32cube_fw...

TYush.1 by Associate
  • 4607 Views
  • 3 replies
  • 0 kudos

I2C MX settings for an LSM303AH

Specifically, settings for the  "Timing configuration" and "Slave Features". The MCU is an STM32L476, Pins are PC0, PC1, PC2, PC3, and PA0 for the SCL, SDA, XL2 INT, XL1 INT, and MAG INT respectively, if that mattters.

JBonn by Associate III
  • 743 Views
  • 0 replies
  • 0 kudos

Why does CubeMX "turn on" HSI if it's not referenced?

This is a bit nit-picky, but it's confusing. For a USB experiment on an STM32F103, I'm seeing an odd clock setting that isn't used and wondering why it is this way. The USB application uses an 8MHz HSE crystal as per usual. RCC_OscInitTypeDef RCC_Osc...

Grant Bt by Senior II
  • 1909 Views
  • 3 replies
  • 0 kudos

TLS protocole with Raw Api LWIP

I want to use TLS protocole on raw api with lwip, how can I start ? I couldnt find any source with raw api. Is this possible or not ? On the cubemx , I couldnt select lwip+tls without freertos

DCtech by Associate II
  • 1109 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L4Q5VGTxP DMA why it doesn't work.

STM32L4Q5VGTxP I use the board I made.FUNC 1) HAL_SPI_Transmit(ILI9341_SPI_Handle,&data,1,100);The output waveform is observed with SCLK / MOSI PIN.FUNC 2) HAL_SPI_Transmit_DMA(ILI9341_SPI_Handle,&data,1);Output waveform does not appear with SCLK / M...

0693W00000Dq6c2QAB.png 0693W00000Dq6bxQAB.png 0693W00000Dq6beQAB.png
YPark.5 by Associate II
  • 1363 Views
  • 2 replies
  • 0 kudos

FMC configuration for LCD interface

Hello,I am working on STM32F746ZG and I am trying to interfacing a display using FMC peripheral.But actually I can't get it work... My display seems to receive some commands but I can't successfully send color.First of all I used CubeMX to configure ...

0690X000009YvGeQAK.png 0690X000009YuXFQA0.png 0690X000009YuXKQA0.png 0690X000009YuXjQAK.png
LGall by Associate II
  • 7059 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.