STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

SMBus-two-wire-Interface unavailable for STM32G474RCT3

Howdy!I'm encountering a peculiar issue using STM32CubeMX ( version 16.6.1 ) and configuring the I2C1 peripheral with firmware version STM32Cube FW_G4 V1.6.1.In short, I'm trying to configure it for SMBus-two-wire-Interface, but this option fails to ...

Screenshot 2026-01-06 at 12.59.52 PM.png
redmore by Associate
  • 414 Views
  • 1 replies
  • 0 kudos

STM32WBA: Dual PDM microphones via SPI interface

Hello,Due to limitations with the STM32WBA's silicon & Bluetooth stack we've had to significantly re-engineer our hardware and add an external Bluetooth chip. As part of this, we updated our SAI blocks so that one block is transmit and one is receive...

JFisherLegato_0-1767195968402.png

Resolved! Changes made in CubeMX 6.16.1 not seen by CubeIDE

Hello,I searched on Google but I don't know if anyone has encountered this problem before. As we know, CubeMx and Cube IDE were recently released as two separate programs. I think this error might be related to that.The error is this: I open a projec...

Resolved! CubeMX Memory Management and NAND_Flash region.

When I used the MMT tool in STM32CubeMX to configure a 256MB NAND FLASH based on FMC, an error appeared. I am using the STM32H743IIT6 chip and have configured NAND FLASH in the FMC. I want to know how to solve this problem. 

PixPin_2025-12-25_22-24-47.png
hhywyh by Associate
  • 599 Views
  • 3 replies
  • 2 kudos

Ioc file destroyed

Yes I should have taken a backup - but modern software must always have build-in backup solution so you do not corrupt your own files. Ask chatgpt if you need the code. I used 2 days to make this project, luckily I have the main.c so I can copy names...

Resolved! How to enable AES/CRYP IN STM32cubeMX

Greetings everyone,Using the C programming language, I'm creating the encryption algorithm AES-256 code for a trusted execution environment and checking to see if the hardware supports it.AES/CRYP enabling is giving me trouble. I can't find it under ...

Nirene_0-1767090537058.png
Nirene by Associate II
  • 823 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.