STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM3N6: CubeMX pin conflicts (false positives)

Hi all, I am trying to get a zephyr project running on an STM32N6570-DK, including Camera, NPU, VENC and Ethernet.I have been using STMCubeMX 6.16.1 to create the project based on the provided DK default settings.For the Ethernet block, the configura...

svogl_0-1767880253394.png svogl_1-1767880552958.png
svogl by Associate III
  • 445 Views
  • 3 replies
  • 4 kudos

Resolved! Cannot assign GPIO into multiple contexts

Using latest STM32CubeMX version 6.16.1 on STM32N6570-DK. It is possible to assign peripherals like UART, I2C, etc. into multiple contexts - boot, app, memloader, but I cannot find a way to assign plain simple GPIO's into multiple contexts. CubeMX on...

MikkLeini_0-1767774307084.png MikkLeini_1-1767774322825.png

Resolved! STM32CubeMX 6.16.0 - STM32H563 - Values not being updated

Hello!I wanted to set up some settings from CubeMX, specifically NX_IP_PERIODIC_RATE in NetXDuo and Rx Descriptor Length in ETH section. NX_IP_PERIODIC_RATE default value is set to 100, but when I set it to 1000, the value does not change when re-gen...

Sander_UP by Associate III
  • 996 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.