STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

STM32CUBEMX doesn't show GPIO Pull-up/Pull-down option for I2C

Hello,I'm trying to imitate an I2C solution. I'm using STM32F100RB.When selecting I2C -> In the example, they have these GPIO settings for I2C pins:Note the GPIO Pull-up/Pull-down option:Here is mine:The CUBE version is identical.The I2C configuratio...

0690X000008a7jqQAA.jpg 0690X000008a7kFQAQ.jpg
ISeed by Senior
  • 7790 Views
  • 11 replies
  • 0 kudos

USB_OTG_FS: Unselsecting "Activate_SOF" doesn't change code.

USB_OTG_FS: In one of two projects unselecting "Activate_SOF" in the .ioc environment doesn't disable its entry in the code! Error of the IDE or is there something else keeping the SOF enabled? As said, in another project it works a as expected. 

0693W00000QOGqVQAX.png 0693W00000QOGs1QAH.png
NRoth.1 by Associate II
  • 2893 Views
  • 4 replies
  • 0 kudos

Resolved! How do we update CubeMx from 6.3.0 to the current version.

We need to update CubeMx from 6.3.0 to the latest version. When updated before, we were told to completly remove CubeMx and start again. This caused all sorts of issues.There must be an easy way to update these days. We can't see any options on the C...

Darcy1 by Associate II
  • 6622 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.