STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H747 no VBUS, USB disk connected via OTG

I'm using STM32H747I-DISCO board to test. I connected OTG adapter and USB disk to CN1 (OTG HS) port.In my STM32CubeIDE I have USB_OTG_FS enabled and configured.The software initialized the driver (successfully), then I try to mount my USB disk and I ...

0693W00000QNryxQAD.png 0693W00000QNrzbQAD.png
HTD by Senior III
  • 2286 Views
  • 2 replies
  • 0 kudos

How to change SPI module baud rate at run time

Hello Support Team,Currently, I am working on the STM32H745-Disc board.In that, I have used the SPI2 module and I have also configured the baud rate as a 3Mbit/s using the STM32CubeMX configuration tool and generated code for the same. (SPI Init done...

HPate.10 by Associate III
  • 2958 Views
  • 2 replies
  • 0 kudos

Resolved! Callback function for HAL_TIM_OnePulse_Start_IT?

How do I get a callback function for the HAL_TIM_OnePulse_Start_IT function?I have a STM32G071 Nucleo board.I whish to start a one-shot timer that calls an interrupt callback function when the time has elapsed. For this I have chosen the timer 6 and ...

FwMaker by Associate II
  • 6015 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.