2022-08-03 7:59 PM
The chip I am using is the stm32H743IIT series. I want to detect the frequency of a signal through GPIOD1, but the external trigger cannot be performed normally. The configuration code is as follows
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOD_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
HAL_NVIC_SetPriority(EXTI1_IRQn,2,1);
HAL_NVIC_EnableIRQ(EXTI1_IRQn);
2022-08-24 2:02 AM
Hi @pwang.2
Can you please provide more information about the issue and if it possible your cubeMx file
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.