STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! "HAL_ADC_Start_DMA()" - init MSP bug

I am working on a STM32f030.I need to convert 2 channels of ADC, and decided to use DMA.After reading the "HAL ADC Generic Driver" - UM1785 section, I got the idea that I don't have to use the "HAL_ADC_MspInit ()" function.However, nothing works unti...

What other code portion(using code generation) changes apart from SystemClock Config replacement with clock setting changes

Hello, I am using STM32CubeMX to generate the code and test some peripherals which runs at different clock speeds(optimally).Since there is lot of code I have (specific to application) post STM32CubeMX code generation being written I don't want to re...

darla14 by Senior
  • 2613 Views
  • 4 replies
  • 0 kudos

How to setup gitlab ci for STM32CubeMX?

Hi guys,I am very new to continuous integration. My company has tasked me to set up a gitlab ci for there STM32CubeMX project. They want the following:A self hosted gitlab on a docker container on a machine (This I have already set up)Gitlab runner o...

Tamper button does not work on cm4

I am using an STM32H757-eval board. From the CM7 I can detect a Tamper button press (PC13). I would like to detect this same button press from the CM4. Using CubeMX, I assign PC13 to the CM4. After rebuilding, I am not able to detect Tamper button pr...

Gil1 by Associate III
  • 3777 Views
  • 8 replies
  • 0 kudos

Multiple adc conversions using DMA (help please)

1.volatile uint16_t ADC_Value[4];-this is my array for the values to be stored2.void ADC1_Configure(void) {  ADC_InitTypeDef ADC_InitStructure;     ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;  ADC_InitStructure.ADC_ScanConvMode = ENABLE;  ADC_...

hpark.21 by Associate
  • 1472 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.