STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

FreeRTOS code generation bug on V6.7.0

Hello,After creating a blinky project in CubeIDE version 1.11.0 running on Linux and setting up FreeRTOS within the .ioc file, the default task fails to run.A project created with STM32CubeMX V6.6.1 works, but when it was migrated to V6.7.0 (by openi...

NWrig.2 by Associate
  • 1962 Views
  • 2 replies
  • 0 kudos

STM32CubeMX bug? MX_DMA_Init() called in the wrong order.

I'm setting up the DMA to move received bytes from USART3 to a circular buffer. But the DMA don't move the received data to the buffer. The received data is received by USART3 (The DR contains the received byte and SR.RXNE is set to 1).All I need to ...

MSipo by Senior II
  • 2040 Views
  • 3 replies
  • 0 kudos

CubeMX " Not a valid ioc file" error

Hi,I have installed STM32CubeMX v6.7 on my laptop. The installation was successful.Loaded a project which was setup with STM32CubeMX v6.3 using FW_GO v1.5.0.The code is generated successfully, however when pressing to open the project, " Not a valid ...

Adole.1 by Associate
  • 2880 Views
  • 3 replies
  • 0 kudos

STM32F7xx Eth with CubeIDE Update 1.11.0

I have wrote an product with tcp communication, last modification September 2021...Today I need a small evolution ( move from HSI-RC to HSE)...the Ethernet does not run now.I have try to work with doc concerning the new driver versus legacy...help-me...

EBAHI.1 by Associate II
  • 2009 Views
  • 3 replies
  • 0 kudos

Resolved! Failed STM32 Cube HAL for OLED SSD1306 with SPI

I'm configuring a STM32F205RET for SPI: hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init....

0693W00000Bci7QQAR.jpg 0693W00000Bci6wQAB.png 0693W00000Bci7BQAR.png

Resolved! NO ADC DMA interrupt on F446RET6, CubeMX 6.7.0, FW4_1.27.1

Hello!I have faced the problem with ADC checking using DMA on my F446RET6 MCU. The software tools are CubeMX 6.7.0 and CubeIDE 1.10.1. The Firmware is FW4_1.27.1. Perhaps, it is my mistake, but i canntot understand how to fix it. Here is the simple p...

sfrwmaker by Associate II
  • 1249 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.