STM32CubeIDE for Visual Studio Code (MCUs)

Ask questions on the STM32CubeIDE for Visual Studio Code extension. Find answers on a variety of topics, including build issues, debug functionalities, CMake project integration, and feature requests for CubeCLT installation.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U073CCTX SVD File?

Trying to debug my code in VSCode using the Cortex-Debug extension, however, I cannot seem to locate the SVD file for the STM32U073CCTx MCU. The CAD Resources tab for the STM32U073CC does not show anything other than footprints.  Any ideas where I ca...

KoKoTee by Associate
  • 4798 Views
  • 6 replies
  • 8 kudos

Resolved! Cube pack sync error via vscode proxy

Hello! I installed the extension and configured it to work through a proxy (downloading the compiler, etc.), and everything works fine, but when I try to download devices list via cube pack sync, I get the error: Failed to download with Unsupported `...

Wyrm by Associate II
  • 877 Views
  • 3 replies
  • 2 kudos

Resolved! New VSCode Extension flash task

Hi,In the old VSCode extension there was a task called something like "Erase + Flash" which would flash the board and then the program could run. After updating, there is now no such task so the only option is to flash the board by debugging. Is ther...

sasodoma by Associate
  • 956 Views
  • 3 replies
  • 2 kudos