2024-05-07 5:22 PM
Trying to debug my code in VSCode using the Cortex-Debug extension, however, I cannot seem to locate the SVD file for the STM32U073CCTx MCU.
The CAD Resources tab for the STM32U073CC does not show anything other than footprints. Any ideas where I can find the file? Are there any alternatives I can use in the mean time?
Solved! Go to Solution.
2024-05-07 6:19 PM - edited 2024-05-07 6:26 PM
Perhaps can find in Keil packs
The .pack is a .zip internally
STM32U0xx_DFP\1.0.0\CMSIS\SVD\STM32U073.svd
2024-05-07 6:19 PM - edited 2024-05-07 6:26 PM
Perhaps can find in Keil packs
The .pack is a .zip internally
STM32U0xx_DFP\1.0.0\CMSIS\SVD\STM32U073.svd
2024-05-20 4:29 PM
Hi Tesla DeLorean,
Following up on the above file, it appears that not all modules are defined in the .svd file for the STM32U073CC. Is there an update to the file? Is it possible to add the missing modules (eg. TIM16, TIM17) manually into the file?
Thanks,
KoKoTee
2024-05-20 5:26 PM
@STOne-32 @STTwo-32 can someone action this for review?
2024-05-21 8:19 AM
2024-05-21 10:07 AM
Hello @KoKoTee @Tesla DeLorean ,
Thank you for bringing this issue to our attention.
I reported internally.
Internal ticket number: 181925 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-16 6:14 AM - edited 2025-10-16 6:15 AM
Hello all;
After checking TIM17 isn't supported in STM32U073. You can find the fix under RM0503 Rev4.
Also the TIM16 issue in svd file is solved.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.