STM32 MCUs
From FAQs to complete How-to articles, find useful articles on STM32 MCUs programming, troubleshooting, ecosystem, and product details.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge base articles

How to implement USB mass storage device standalone on STM32

Introduction This article provides a detailed, step-by-step guide to implementing a USB mass storage class (MSC) device using the USBX middleware in standalone mode (without an RTOS) on the STM32U5 microcontroller. The example is developed and tested...

FBL_0-1758562183659.png FBL_1-1758562183661.png FBL_2-1758562183664.png FBL_0-1758566670769.png
FBL by ST Employee
  • 4191 Views
  • 0 comments
  • 1 kudos

How to configure VREFBUF on my STM32

The voltage reference buffer embedded in most STM32 devices serve two main purposes: 1. used as a voltage reference for ADCs, and DACs 2. used as a voltage reference for external components through the VREF+ pin Note that as each product family is un...

1005.png 1006.png 1007.png 1008.png

How to obtain and use the STM32 96-bit UID

Introduction Some STM32 MCUs embed two unique identifiers: a unique 96-bit unique identifier and device ID. This article shows how to both obtain these values in your code, and describe some possible use cases for them. 1. 96-bit unique ID This 96-b...

BMontanari_3-1758715277406.png BMontanari_1-1758715035836.png BMontanari_2-1758715156791.png

Internal clock CK_INT for the STM32H7/H5 timers

Introduction to CK_INT clock  The STM32 products include a flexible clock system for timers, enabling each timer to operate with a specific kernel clock. The RCC configuration determines the kernel clock source for each timer.Timers can utilize vari...

SarraS_0-1757685323191.png SarraS_0-1757674890870.png
Sarra.S by ST Employee
  • 1834 Views
  • 0 comments
  • 0 kudos

How to use semihosting with STM32CubeIDE and STM32

Summary Semihosting can be used to enable code running on STM32 to communicate with the host computer during a debug session. This makes it possible to use host computer I/O (for example keyboard, display, or file system) instead of having such input...

1565.png 1567.png 1570.png 1571.png
LauraCx by ST Employee
  • 30621 Views
  • 6 comments
  • 5 kudos

How to connect two quad-SPI memories using only one OCTOSPI

There are two possible solutions for connecting two quad-SPI memories using only one OCTOSPI interface. Solution 1: Use a dedicated bit in the OCTOSPI_CR register for external memory selection: MSEL bit for STM32H5, STM32U5, and STM32L5 series or FS...

KDJEM1_0-1719503650093.png KDJEM1_0-1721138414681.png
KDJEM.1 by ST Employee
  • 5115 Views
  • 5 comments
  • 4 kudos

How to use the LPAWUR range on the NUCLEO-WL33CCx board

The low power wakeup radio (LPAWUR) feature is not enabled by default on NUCLEO-WL33CCx boards. It has been designed for the reception of a specific frame to trigger the wake up of a system. To enable and use the LPAWUR feature on the NUCLEO-WL33CCx ...

ImenD_0-1756476306474.png
Imen.D by ST Employee
  • 1207 Views
  • 0 comments
  • 1 kudos

Reset management on the NUCLEO-WBA55CG

The NUCLEO-WBA55CG with MB1801-NoUSB-D02 has a different configuration for reset management compared to earlier versions. In the default configuration, the reset via mass storage and the reset via debugging tools are disabled, which may cause issues...

STTwo32_0-1756286143499.png
STTwo-32 by ST Employee
  • 1165 Views
  • 1 comments
  • 1 kudos

How to set up Sigfox on STM32WL3x

Introduction This article explains how to set up Sigfox connectivity on the STM32WL3x microcontroller. Sigfox is a low-power wide-area network (LPWAN) technology designed for IoT applications requiring long-range and low-energy communication. By fol...

STTwo32_0-1755877750148.png STTwo32_3-1755879403567.png
STTwo-32 by ST Employee
  • 1028 Views
  • 0 comments
  • 0 kudos