STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Issues with LoRa Nucleo Pack

Having checked the ST Website for LoRaWAN kits I settled on the LoRa LF Sensor and Gateway kit (P-NUCLEO-LRWAN3) There is no mention on the website that this pack is obsolete or end of life. I always check that because I have been burned before by ST...

Screenshot 2025-06-05 at 11.54.04.png
KMill by Senior II
  • 3035 Views
  • 7 replies
  • 5 kudos

Resolved! BLE stack reset

In my project STM32WB55 uC is used and FW is generated by STM32CubeMX.Library (STM32Cube_FW_WB_V1.22.0) and BLE binary (stm32wb5x_BLE_Stack_full_fw.bin) are both version 1.20.My goal is to reboot only BLE stack on CPU2 without reset of CPU1.On commun...

strahinja by Associate II
  • 2496 Views
  • 7 replies
  • 1 kudos

Resolved! STM32WBA 32MHz HSE. Can't Initialize HSE

Hi,I made a custom PCB with a STM32WBA54CGU6 to act as a Bluetooth LE Audio transmitter. This was going to be first "real" PCB since before I have only made much simpler designs (I know I was very ambitious). For the HSE, I used this document to deci...

Pablo04_0-1748819756112.png
Pablo04 by Associate
  • 1194 Views
  • 2 replies
  • 0 kudos

Resolved! BLE sleep advertising at fast rate of 1 or 2 ms

Got this issue on entering sleep. I set my advertising to 1 second, and do not touch it after. Before sleep, all was good,  I was advertising every ~1 second but when I enter sleep I notice it jumps to 1 or 2 ms.. very fast, and not so power consumin...

DS.4 by Senior II
  • 2136 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.