2025-05-13 12:49 AM
Hello,
I built two PCBs, one with the STM32WL33KCV6TR (QFN32 version) and one with the STM32WL33CCV6TR (QFN48) version. Both schematics are identical (48MHz + 32768Hz crystal connected, SMPS used, decoupling capacitors on power pads, otherwise nothing is connected to the chips). On both versions I flashed the PWR_DEEPSTOP_RTC example. On the *CC* the original version from the example library, on the *KC* I used cubeMX to change the .isc file to the *KC* version. Afterwards I used a diff tool to make sure both project folders are identical (apart from the KC/CC difference).
My expectation would be that both PCBs draw the same amount of current.
However during "active" time in the software example the CC current draw is 4.3mA vs 3.0mA of the KC version.
During deepstop the CC version draws 1.3mA while the KC version draws the expected 1.2µA.
These measurements have been done at 3.3V.
Here are more measurements.
| active | deepstop | |
| STM32WL33KCV6TR @ 3.3V | 4.3mA | 1.3mA |
| STM32WL33CCV6TR @ 3.3V | 3.0mA | 1.3µA |
| STM32WL33KCV6TR @ 1.8V | 4.3mA | 740µA |
| STM32WL33CCV6TR @ 1.8V | 3.7mA | 1.2µA |
All tests have been done with cubeIDE 1.8.1 on MacOS with FW 1.1.0.
Especially during deepstop the power consumption of the KC variant is far too high.
Is there any register setting I need to change for the KC variant to reduce the power consumption or anything else that needs to be different between these two versions?
Thanks!
2025-05-26 7:19 AM
Hello @jaaarp
Could you please reproduce the same test using the PWR_DEEPSTOP_RTC as it is on both MCUs. I think it should work for both of them.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-28 10:53 AM
Hello @STTwo-32 In the example overview of cubeMX and cubeIDE I find the PWR_DEEPSTOP_RTC example for the CC variant but not for the KC variant. Where can I get to KC variant of the example to run it as it is? Thanks!
2025-05-28 11:24 AM - edited 2025-05-28 11:24 AM
There is not an example for such a variant. The same example should be able to work on both variants.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-30 6:55 AM
2025-06-05 1:24 PM
Hi @STTwo-32 I got what you meant now and flashed the compiled binary from the example for the CC variant on the KC variant. There the system behaves like expected with a power consumption of 1.2µA@1.8V during deepstop. This means the PCB circuit is fine but something went wrong with porting the example from the KC variant to the CC variant. What is the correct way to do that or is there anything to pay attention to when changing the chip variant with CubeMX? Is there any example project I can use for the CC on which I can build an application with LPAWUR and MRSUBG that correctly goes into deepstop? Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.