NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello ST community,Just thought of buying NUCLEO-WL33CC1 for development of flight telemetry. But I have few doubts before buying.1. What is the radio coverage distance with the default antenna that comes along with the kit? Assuming the test area is...
Hello, I am a beginner following this official ST tutorial: https://www.youtube.com/playlist?list=PLnMKNibPkDnFPqEmJAwEjsSS8MOQZHRNF I am trying to assign specific GPIO pins (for a BUTTONs and an LEDs) to a specific core. However, when I right-click ...
Hello everyone, I'm currently working on several projects on STM32Cube IDE with each of them implementing the different low-power modes available on the Nucleo-WL55JC1 board (Sleep, LPR, LPS, STOP0-1-2, Standby and Shutdown).For each of them, I follo...
My current project is a small (15 x 30 mm) PCB, with 4 layers. I use the STM32WB1MMC module for BT connectivity. Are there things to consider when designing this 4-layer PCB in order to maximize BT range?Thanks!
Hello,I'm a beginner on CubeIDE but I want to learn how to use the BLE from the STM32WB55 Nucleo Board. I've been following several tutorials throughout the web, from ST and others, such as https://www.youtube.com/watch?v=i10X4Blr8ns or https://www.y...
It's quite annoying that the names of the BLE stack are cut off, even though there's plenty of free space. The browser doesn't matter. My screen resolution is 2496 x 1664, with 150% scaling on Windows.
Hello everyone,I was trying to build communication between 2 LoRa devices. Sending a "Hello" from Tx board and receiving on Rx board. I tried to debug using UART (printf through Tera Term). But I am stuck at transmitting data. Do any of you have an i...
Hello,I'm having problems with the FUS not starting and the Wireless stack not responding.In my code, the wireless stack can be updated. In the process of updating it, the STM32WB55 was interrupted by an external reset, and the FUS was left unrespons...
After performing an OTA update, the Bluetooth icon appears as shown in Figure 1, but it does not display the "STM_OTA" name.The correct result should look like Figure 2.I followed the modification steps from this video, including adding the OTA Rebo...
Dear Team, May I know STM32WBA52CG support some basic AI/ML applications. We don't need controllers like STM32N6. If STM32WBA52CG supports some basic AI/ML can you please share some materials,applications notes or some examples where I can see some A...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.