NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I'm trying to connect an OLED display to my STM32WL55JC by I2C but it doesn't work...I've successfully connect it with a STM32F411RE but the I2C configuration / HAL interface seams to be different between both MCU...Here my config on the STM32...
Can you use the extended advertising and scanning found in BLE 5 somehow? I have found some references to them in the code, but cannot find any defines. Do they exist? Will they be implemented?
In examples I got familiar with RF low level access is controlled by some exact coprocessor firmware. Existing coprocessor binaries provide some higher level of abstraction that seems to not include forcing signal with exact characteristics. Do I mis...
Hi, I want to use B-U585I-IOT02A as a controller for mobile robot, I use a smartphone for the remote control. For now I am using HC-05 as the bluetooth interface because I can't find out how to program the STM32WB5MMG to act similar with HC-05. Can a...
I went from the v1.12.1 stack to the v1.13.3 stack and LE Privacy seems to be no longer working. It advertises, but always with the static random address, not a random resolvable address. Also, the address never changes. Anyone else seeing this? ...
Hello, Can you please point me to the factory settings of stm32wb55 pucleo board.I seem to have erased some sectors 1-192 and fiddled with some option bytes (nBOOT0) and nSWBOOT0Best Regards,D
Several BLE circuit design inquiries of the STM32WB55RG MCU.The BLE impedance requirement of this MCU is 50 ohm, and it is recommended to use LPF (MLPF-WB55-01E3). For the detailed circuit diagram, please refer to the fourth page of the attached file...
STM32WB55RGV6 connects ADS1299 by spi. And I choose spi2. There are three signas miso\ mosi and sck. SPI2 has two alternative: GPIO_AF3_SP2 and GPIO_AF5_SPI2.① STM32CUBEMX automatically generated miso(GPIO_AF3_SP2), mosi and sck(GPIO_AF5_SPI2).Initi...
I was trying to use the time server for a project on STM32WB55. I tried to use it in an empty project. When I tried to debug, this window pops up:The curious part of the problem is that this error seems to happen with the time cluster only: using ano...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.