STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

BLE PairingTime

Hello, I have a BLE Secure Connection implemented between an android phone and STM32WB55. Currently, using fixed key to start pairing, it takes approximately 2 seconds to get paired (after the key is sent, and devices are paired) in addition to 600ms...

Amogh by Associate III
  • 2006 Views
  • 2 replies
  • 0 kudos

STM32WLE5CC goes into unknown state

We have developed battery operated product using STM32WLE5CC.when device goes into deep sleep around 1.7uA current are flow normally.During Testing of product we face an issue which is described as below.During deep sleep of STM32WLE5CC, we removed b...

DBhut.1 by Senior
  • 1276 Views
  • 2 replies
  • 0 kudos

TIMx_RCR IRQ?

I am using TIM16 as a one second counter on an STM32WB55. I would like to generate an interrupt after it rolls x times (as example 2). I set the TIMx_RCR to a 1. Can someone tell me what function I need to call in the HAL library and should I plac...

SWenn.1 by Senior III
  • 892 Views
  • 2 replies
  • 0 kudos

Resolved! I can't run or debug my CM0+ with NUCLEO-WL55JC1.

I have no problem to flash or debug the CM4 of the board. But when I'm trying to flash the CM0+ this error occurred : Error in final launch sequence:Failed to start GDB serverFailed to start GDB serverError in initializing ST-LINK device.Reason: (255...

HPERNET by Associate II
  • 15789 Views
  • 10 replies
  • 0 kudos

Problem flashing STM32WLE5J8I6, stuck at 97%

Hi all. I've got a problem when trying to flash the STM32WLE5J8I6.I am trying to run a simple blinky code and blink an onboard LED on my custom pcb.The program builds fine, connecting with the ST-Link (Nucleo-WL55JC1) and using SWD to connect to the ...

0693W00000NpB6iQAF.png
Cvan .7 by Associate II
  • 2066 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.