2019-10-21 6:05 AM
Can you use the extended advertising and scanning found in BLE 5 somehow? I have found some references to them in the code, but cannot find any defines. Do they exist? Will they be implemented?
2019-10-21 8:38 AM
No the STM32WB RF stack is not supporting this optional BLE 5.0 feature and it will not be supported .
But it will be supported in the next member of the ST wireless device family.
2022-02-25 2:51 AM
Hi @Remi QUINTIN Is this feature now available in STM32WB55?
2022-03-04 8:32 AM
Yes this feature is now available in the last WB FW packages starting from v1.13.0. In the release notes: BLE new features => Extended advertising (under application flag selection)
2022-03-04 11:10 AM
@Remi QUINTIN - the v1.13.2 BLE_HeartRate sample application does not run if I use the
stm32wb5x_BLE_Stack_full_extended_fw.bin
What sample app is configured to be able to run with that new library?
I don't know where to find scatter file referred to in release note, but not explained anywhere I can see:
BLE:
2022-03-04 11:29 AM
Ok, so it looks like the stm32wb5x_BLE_Stack_full_extended_fw.bin library is not usable by the common customer until sample apps support it in v1.14.0:
P.S. ST, maybe it would have been better to not include it in the public release for common customer before then ;-\
2022-03-11 6:22 AM
Hi @Remi QUINTIN the following thread says it's not available.
I think STM shouldn't release such information until they have actually built it. Now, I have been struggling with this and our product test and launch data has been postponed. Please make sure to add correct information in release notes.
2022-05-12 12:56 AM
Hello, I have one additional question related to advertising or extended advertising. Is/Will be there possible to make configuration based on the BLE stack that device is broadcaster and observer in one?
I know that this is probubly not standard using of bluetooth, so it's just the questino of possibility.
Is there already set exact date of stack update to support extended advertising?
Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.