STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32CubeMX generate "feature not supported" instead ...

The STM32CubeMX generate:```#define LCD_SPI_Send_DMA(rd, ln)           BSP_ERROR_FEATURE_NOT_SUPPORTED```instead if I modify the generated DISPLAY/Target/lcd_conf.h with`#define LCD_SPI_Send_DMA BSP_SPI1_Send_DMA`seems work correctly.I am using:Nucle...

NRoss by Associate II
  • 2345 Views
  • 4 replies
  • 0 kudos

STM32: consumption due to I2C in stop2 mode

Hi, I use the nucleoWL (STM32WL which is based on STM32L4). I want to use LPWAN to communicate some measurements each day. I use I2C between MCU and sensors. If I try the Sigfox Push Button exemple, I have 2uA in stop2 mode but if I add I2C1 (thanks ...

0693W00000JP7OGQA1.png 0693W00000JP7QlQAL.png
LLr.1 by Senior
  • 1684 Views
  • 2 replies
  • 0 kudos

Resolved! Restore ST-Link Connection on B-L072Z-LRWAN1

In order to achieve minimum power drain on the B-L072Z-LRWAN1 discovery board, it is necessary to remove some solder bridgesSee: https://community.st.com/s/question/0D50X00009XkbSOSAZ/excess-current-consumption-running-bl072zlrwan1-from-batteryAnd:ht...

0693W00000NpgutQAB.jpg 0693W00000Npgv3QAB.jpg

Resolved! Cant power B-L072Z-LRWAN1 with battery

We recently received our B-L072Z-LRWAN1 but are not able to run the program while batteries are plugged in. In the datasheet it says that we need to remove SB37 to accomplish this. But then I cant program it anymore? How can I use the board with batt...

KPage by Associate
  • 14930 Views
  • 26 replies
  • 1 kudos

Resolved! STM32WB55 color control cluster gives an assertion error. assertion "zigbee_app_info.colorControl_server_2 != NULL" failed.

As I said, I get the assertion "zigbee_app_info.colorControl_server_2 != NULL" failed error from a standard debug function in the code.I thought it could have something to do with this struct, which is a bit above it.struct ZbColorClusterConfig color...

STM32WL55CC LPUART1 to UART1 freeze

Hello everyone,I work on a project with LSM100A whitch integrate an STM32WL55CC.I have an SDK available to start development and in this SDK, we can find debug information on LPUART 1 (PA2,PA3).For my project, i can't use LPUART1 so i have decided to...

MLam by Associate III
  • 1927 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.