STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! why two inductors for SMPS on P-NUCLEO-WB55

There are two inductors, L1 10uH and L5 10nH, in series for SMPS circuit in P-NUCLEO-WB55 design. Why is that? is the sequence affective (smaller L5 coming out of VLXSMPS pin)? Thanks. -wq

0693W00000aIbk1QAC.jpg
WQ by Associate III
  • 1661 Views
  • 3 replies
  • 0 kudos

Bug for BLE Init in new wb5 firmware 1.15

I've used BLE for a month now on the wb5mmg with the 1.14.1 firmware with the steval-proteus board. The setup in the .ioc for new projects was always the same:HSEM, IPCC, RCC, RTC, RF, (USART)Activating BLEUsing Default P2P Settings or Custom Templat...

0693W00000WKe8SQAT.png
Lotta by Associate II
  • 6733 Views
  • 13 replies
  • 0 kudos

STM32CubeWL v1.3.0 - General questions on the examples

Hello,we’re doing some research on LoRa tecnology to evaluate if it’s suitable for our products. We’re interested in STM32WLxx MCU, so we downloaded STM32CubeWL Firmware package from GitHub.We are trying to understand the principle of working of some...

0693W00000aJeCYQA0.jpg 0693W00000aJeCdQAK.png
GGhet.1 by Associate
  • 1805 Views
  • 1 replies
  • 0 kudos

Resolved! The simplest and most basic LL driver App doesn't work

We tried the simplest and the most basic LL driver based App, LED blinking, on Nucleo boards:int main(void) { LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG); LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR); NVIC_SetPriorityGrouping(NVIC_PR...

WQ by Associate III
  • 5519 Views
  • 11 replies
  • 0 kudos

How create devEUI for public Lora network?

I have one product with inside the module Murata CMW. The product will be present on a public Lora network. The product is a sensor, so it will trasmit dataI need to go in mass production and I need to create the devEUI for each deviceHow I can creat...

FSogn by Associate
  • 2380 Views
  • 2 replies
  • 0 kudos

STM32WL55 as single chip 4-fsk transceiver

Hi, I'd like to understand how I can setup the semtech transceiver to work with 4-FSK modulation. I configured a project in cube mx but I have doubts on the bandwidth and datarate parameters.I know that my datarate is 9600 bps, then bandwidth and cod...

ltoso.1 by Associate II
  • 2378 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.