2019-03-18 7:09 AM
I have one product with inside the module Murata CMW. The product will be present on a public Lora network. The product is a sensor, so it will trasmit data
I need to go in mass production and I need to create the devEUI for each device
How I can create it?
I see there is method to create the devEUI from a MAC address (that I have avaiable), but it's deprecated
The method is use one MAC adding FF and FE on the 4th and 5th byte and turning to 1 the 7th bit of first byte.
Is there other valid method to create the devEUI witout problem?
2023-03-23 7:56 AM
Hello,
I have same problem, we have been having an OUI for many years for mac adresses, can we can use for DevEUI ?
Did you answer to that question ?
Is it necessary to register in https://standards.ieee.org/faqs/regauth/ ?
2023-03-23 9:26 AM
Register the LoRa Raspberry-Pi Gateway on The Things Network (TTN)
Go to www.thethingsnetwork.org to create an account.
Log in to the TTN account and follow instructions for registering the LoRa gateway. Make sure to check the box “I'm using the legacy packet forwarder.�? Note: One account can support multiple gateways.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.