NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
One of the biggest offenders is shown in the image below. All of the USB device types from usbd_def.h are not getting recognized by the compiler, even though usbd_def.h is in the include list at the top of the file in this image, and I can control-cl...
Hello, to get a lower power consumption in my application i would like to go in stop mode 2 and wake up shortly to receive some characters on the LPUART. But unfortunately my mcu does not wake up. I can see with the debugger that the send Byte is in ...
I would like to create a script by arduino IDE that allows me to communicate in Sigfox. I own an STM32WL55. I haven't found any library on the internet that allows me to do this communication. Is there any documentation explaining how to program this...
Hello, I am trying to create a simple openthread project on my NUCLEO-WB55RG. There is no custom code in this project; just the code generated from the CubeMX ioc file attached.By all means, I think that I have all the necessary settings for this pro...
I can make the RTC wakeup work in Standby mode, but not STOP2 mode.
i am working with lsm303agr accelerometer and magnetometer sensor module with controller STM32WB , am using the library from the ST for the implementation of software. I can able to fetch data using the I2C protocol. But when I try to use the SPI 3 w...
Hi fellas,We are planning for LoRa based FUOTA updates using STM32 MCUs. The LoRa Transceiver we are planning to use is SX1302. In I-CUBE-LRWAN blog, they told its meant for STM32L0/1/4 series alone. Can we use some other series like STM32G0 series, ...
Hello togetherI am currently doing the tutorial from ST (STM32WB Getting Started Series: Part 12b, Lab. Receiving data from the phone) to send and receive Information with BLE. I am stuck in the video at 15:00 when the device should show up on the ST...
Say I want the Projects/B-L072Z-LRWAN1/Applications/LoRaWAN/LoRaWAN_AT_Slave project loaded up.What exactly am I supposed to do in the IDE?I've loaded that project up, but can only build the debug configuration - it doesn't seem right.I did change th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.