cancel
Showing results for 
Search instead for 
Did you mean: 

why two inductors for SMPS on P-NUCLEO-WB55

WQ
Associate III

There are two inductors, L1 10uH and L5 10nH, in series for SMPS circuit in P-NUCLEO-WB55 design. Why is that? is the sequence affective (smaller L5 coming out of VLXSMPS pin)? Thanks. -wq0693W00000aIbk1QAC.jpg

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
WQ
Associate III

It is mentioned in AN5165. -wq0693W00000aJggaQAC.jpg

View solution in original post

3 REPLIES 3
AlbertoGarlassi
Associate III

Maybe because bigger inductors have bigger parasitic capacitance and losses at high frequency. In this schematic L5 works OK for the higher armonic content of the PWM and for these frequencies it isolates L1. I guess efficiency is somewhat higher.

L5 should be closer to the switching pin, in this way capacitance to ground is minimized.

AScha.3
Super User

i think, the L1 and L5 are there for :

L1 is for the smps , power inductance;

L5 is EMV related, because this chip has BT receiver and so any noise in the 2.4GHz range should be suppressed.

If you feel a post has answered your question, please click "Accept as Solution".
WQ
Associate III

It is mentioned in AN5165. -wq0693W00000aJggaQAC.jpg

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.