NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
First of all, I was doing basic HAL_UART communication with lora modules. Now I have a new project which requires really really low power so I decided to go with stm32wl.I will have 50 end node device (sensor device) and 1 base station. Sensor device...
I am experimenting with the STM32WLE5 and the embedded SX126 LoRa-radio. (aka SubGHz)I simply reset the SubGHz, then read its status, and this always returns a 'Failure To Execute Command' (according to section 13.5.1 GetStatus from SX126 datasheet) ...
Hello,Currently I am working on STM32WL55JC single core where I initialized PB3, PB4, PB5 and PA15 for SPI1 line with a FLASH Memory MT25QL.I tried basic with reading Flash memory ID.It worked when i used the SPI_FullDuplex_ComPolling_Master example ...
Hello everybody .I am using openthread in a project. I am creating an openthread network using the stm32wb processor. I install the MTD stack software on the slaves I choose from my cards because I always want them to be child. Everything works fine,...
I used STM32WLE5JC control for playing the song via I2S. I have used SPI2 (alternat function of I2S) in the STM32WLE5JC. I can read the song in SD card and transmit the signal to the I2S in the I2S module (MAX98357A). The signal is transmitted to the...
Hello, I need to send data from STM32WB Nucleo to the computer (any symbol), I spend many days, but didn't find any simple example for that in Google. I was surprised usually I never had a problem like that... Please, can you share a simple example o...
Learning how to use the STM32WB55RG alongside the 'Mastering STM32' by Carmine Noviello. I followed the instructions for setting up interrupts to use the NUCLEO hardware buttons, but when I build, I get a warning that 'HAL_GPIO_EXTI_Callback' defined...
Hi,Is there any way to put STM32WB to stop1 mode, without using sequencer, while BLE advertising is on? I know how to enable stop1 and I know how to enable advertising. But how to combine it? I'm exploring the BLE_Peripheral_lite sample. In BLE_Hea...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.