NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
There some limitations/issues with the generation of the LoRaWAN/Target/radio_conf.hThe template radio_conf_h.ftl is hard coding key values in a way that does not preserve user set values.The following lines are of concern:#define XTAL_DEFAULT_CAP_VA...
I just started using the stm32cubemx tool and I want to make an application with a STM32WL55 which only wakes up once every day and exchanges one simple LoRa class A message. I need to use as little power as possible. I get the impression that the le...
data on serial monitor tera term setting what is the reason of data mis matching ?
when i use the adc oversampling code then it work in debugg mode but when i use the heart rate sensor program then it will not work in live debugging ,it say target not found.what is wrong with this code ?
when i generate the adc based code then it show the error without doing anything in the main code
Hi,I am developing an application on the STM32WB10 where multiple smartphones can be connected at once (so far just two but that might change in the future). I can get the handles for each connection, but I also need to be able to send a notification...
Hello,We are having an issue updating the BLE FW v1.13.3 to 1.17.2 using FUS 1.2.0.Everything is working as expected until (after SHCI_C2_FUS_FwUpgrade(0, 0)) we are polling for SHCI_C2_FUS_GetState()At first, its FUS_STATE_VALUE_FW_UPGRD_ONGOING as ...
Is it possible or advisable to use the tcxo as the clock source in a lora end node application? The default configuration in the Lora end node example code uses the MSI as the clock source but surely the tcxo would be a better and more stable option...
HiWhether BlueST-SDK tool is compatible with bootloader STM_OTA dedicated to STM32WB55 ?I using Nucleo STM32WB55 and bootloader from STM (STM_OTA). For update firmware I using for now STM32CubeMonitor-RF and stm32WB USB DONGLE (which is part of nucle...
Dear all,I would like to communicate regarding STM32WB OpenThread Border Router Application.Connectivity:STM32WB OpenThread Border Router Application - stm32mcu (stmicroelectronics.cn) May I ask would you be available to communicate regarding OTBR_CL...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.