NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello ,I am trying to making a BLE application with triggering external interrupts that came from camera sensor. Normally my interrupt handlers worked just fine, however when I try to add BLE function, code getting hard fault. Following lines in the...
The standard OTA application is taking up 28kBytes and even the light stack (v 1.16) starts at 0x08021000 on the 256kB models. This leaves 104kByte in between. Does that mean it is not possible to updatet the wireless stack via OTA on those models?
I'm currently working on a project based on transmitting RF.The objective of the project is to develop a system which is able to communicate with another device based on RF transmission.The system has to be able to provide RF communication at a frequ...
Hello, I'm new at developing Wireless applications with the STM32WB and can not find why old data from old commands stays somewhere in my code and affects my new commands sent. Im writing the command strings into Myble_Characteristic_Command with the...
Board: STM32WB55Software: STM32CubeIDE, STM32_WPAN BLE as Custom p2p serverBackground: Have a test bench set up to check entering Standby Mode with additional features we want to use on our project before implementing it. Have been adding in our feat...
Hi Team, Any Transceiver IC support up to 3GHz range in STMicroelectronics? And how to interface with controller.! Thanks and Reguad,Aravind
Hi there. We are planning to develop a product that includes 5-7 server nodes based on STM32WB15, and one client node based on STM32WB55 which should receive notifications from the server nodes parse them, and send data to the PC through USB CDC. Eac...
How do I change the BLE Access Address?(default 0x8e89bed6)LLD can be changed through a function called HAL_BLE_LLD_Configure, but there are no functions to change the channel and access address other than that.Is it possible to change the access add...
Hi,I'm using the Nucleo-WB15CC board to develop a LowLevel and Lowpower BLE application. The application will sleep 1 seccond, wakeup and send some custom data and then sleep again. Is it possible to have OTA support in this kind of application? Are ...
Greetings,I am using Murata Module and LoRaWAN_End_Node project for my project application which I got from STM website . My code is working fine and transmitting data packet successfully with a specific interval of time.Now I want to send another da...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.