2020-09-23 4:31 AM
Hi
Whether BlueST-SDK tool is compatible with bootloader STM_OTA dedicated to STM32WB55 ?
I using Nucleo STM32WB55 and bootloader from STM (STM_OTA). For update firmware I using for now STM32CubeMonitor-RF and stm32WB USB DONGLE (which is part of nucleo kit). Now I would like to do this in other way - other tools, CLI, scripts...
~/Downloads/BlueSTSDK_Python/blue_st_examples $ sudo python3 example_ble_6.py
##################
# BlueST Example #
##################
Scanning Bluetooth devices...
Discovery started.
New device discovered: STM_OTA.
Discovery stopped.
Connecting to STM_OTA...
Device STM_OTA connected.
Connection done.
Features:
No features found.
1) Firmware upgrade
Select an action ('0' to quit): 1
1)node-stm32wb55
Select a firmware ('0' to cancel): 1
Upgrading firmware...
1
<bound method Node.get_debug of <blue_st_sdk.node.Node object at 0x7647b490>>
none
2
Traceback (most recent call last):
File "example_ble_6.py", line 327, in main
upgrade_console.add_listener(upgrade_console_listener)
AttributeError: 'NoneType' object has no attribute 'add_listener'
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File "example_ble_6.py", line 391, in <module>
main(sys.argv[1:])
File "example_ble_6.py", line 346, in main
upgrade_console.remove_listener(upgrade_console_listener)
AttributeError: 'NoneType' object has no attribute 'remove_listener'
Device STM_OTA disconnected.
Exception ignored in: <function Peripheral.__del__ at 0x76572108>
Traceback (most recent call last):
File "/usr/local/lib/python3.7/dist-packages/bluepy/btle.py", line 630, in __del__
File "/usr/local/lib/python3.7/dist-packages/blue_st_sdk/node.py", line 555, in disconnect
File "/usr/local/lib/python3.7/dist-packages/blue_st_sdk/node.py", line 398, in _update_node_status
File "/usr/lib/python3.7/concurrent/futures/thread.py", line 151, in submit
RuntimeError: cannot schedule new futures after shutdown
2023-09-01 7:17 AM
I am seeing this same behavior trying to run `BlueST-SDK v1.4.0` under Python 3.10. I am using the `example_ble_6.py` from master branch ~Nov 2022.
I tried a couple local modifications but can't seem to resolve yet. Connecting to the STM32WB device works...but then it fails when starting upload. It seems like something is wrong with `node.py get_debug()` as this is the function returning `None`.
Given there haven't been any recent commits, I'm not sure if the project is supported anymore. This is too bad because it seems pretty close to working for firmware updates.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.