NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Attached is my demo project for the NUCLEO-WB55RG dev kit.I'm trying to report ZCL_TEMP_MEAS_ATTR_MEAS_VAL when the attribute value is changed (button 3 pressed), but according to wireshark, nothing is send.See app_zigbee.c, line 329I can correctly r...
static void SendTxData(void){/* USER CODE BEGIN SendTxData_1 */uint16_t pressure = 0;int16_t temperature = 0;sensor_t sensor_data;UTIL_TIMER_Time_t nextTxIn = 0; #ifdef CAYENNE_LPPuint8_t channel = 0;#elseuint16_t humidity = 0;uint32_t i = 0;int32_t ...
Hi, I am working with a NUCLEO-WB15CC and can't erase all of the 320 KBytes Flash. When using the STM32_Programmer_CLI the following works perfectly fine:STM32_Programmer_CLI.exe -c port=SWD -e [0 55]but withSTM32_Programmer_CLI.exe -c port=SWD -e [0...
hi all,I'm working on a STM32WB5MMGHX and I have play with p2p demos and otherI'm trying now to build a Battery service with only a battery level caracteristicI've set the caracteristic as shown belowmy custom app event handler is as folow : void Cus...
Hi! So i have a WL55CC MCU that sends a 64 Byte Payload via LoRa to a Nucelo JC1 Board. When I'm sending with a spreading Factor of 7, everything works just fine, but with spreading factor 12 the receiver goes into a timeout mode, although I've set t...
When setting up the project I go to the ST url to get the ID and PAC from: https://my.st.com/sfxp the zip that is downloaded is corrupted and has a size of 0kb. I have done this procedure hundreds of times so I am sure that the problem comes from the...
Sometimes, if in addition to Bluetooth, WIFI is needed in the development of a product, the third module is used. Does ST plan to include WIFI in the e.g STM32W series in the future?
Hello there!I have a request regarding PA matching impedance measurements.We are currently working on the implementation of a VHF pulsar system. Initially, we tested it on the NUCLEO board without incorporating the filtering components (impedance mat...
Hi,I am having a problem with my P-NucleoWB55 development board. When using STMCUBEIDE and trying to run the program, I get the following error.STMicroelectronics ST-LINK GDB server. Version 7.4.0Copyright (c) 2023, STMicroelectronics. All rights res...
Hello communityGateway terminal image shows FSK at channel 9 and 868 frequency.I have downloaded the library code the default set region is Europe and the frequency is 868. And I have made these changes #define USE_MODEM_LORA 1#define USE_MODEM_FSK 0...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.