2023-11-07 9:06 PM
static void SendTxData(void)
{
/* USER CODE BEGIN SendTxData_1 */
uint16_t pressure = 0;
int16_t temperature = 0;
sensor_t sensor_data;
UTIL_TIMER_Time_t nextTxIn = 0;
#ifdef CAYENNE_LPP
uint8_t channel = 0;
#else
uint16_t humidity = 0;
uint32_t i = 0;
int32_t latitude = 0;
int32_t longitude = 0;
uint16_t altitudeGps = 0;
#endif /* CAYENNE_LPP */
// EnvSensors_Read(&sensor_data);
temperature = (SYS_GetTemperatureLevel() >> 8);
pressure = (uint16_t)(sensor_data.pressure * 100 / 10); /* in hPa / 10 */
float Temp = Get_temperature(); // function reads temperature from sensor
AppData.Port = LORAWAN_USER_APP_PORT;
#ifdef CAYENNE_LPP
CayenneLppReset();
CayenneLppAddBarometricPressure(channel++, pressure);
CayenneLppAddTemperature(channel++, temperature);
CayenneLppAddRelativeHumidity(channel++, (uint16_t)(sensor_data.humidity));
if ((LmHandlerParams.ActiveRegion != LORAMAC_REGION_US915) && (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AU915)
&& (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AS923))
{
CayenneLppAddDigitalInput(channel++, GetBatteryLevel());
CayenneLppAddDigitalOutput(channel++, AppLedStateOn);
}
CayenneLppCopy(AppData.Buffer);
AppData.BufferSize = CayenneLppGetSize();
#else /* not CAYENNE_LPP */
humidity = (uint16_t)(sensor_data.humidity * 10); /* in %*10 */
AppData.Buffer[i++] = AppLedStateOn;
AppData.Buffer[i++] = (uint8_t)((pressure >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(pressure & 0xFF);
AppData.Buffer[i++] = (uint8_t)(temperature & 0xFF);
AppData.Buffer[i++] = (uint8_t)((humidity >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(humidity & 0xFF);
if ((LmHandlerParams.ActiveRegion == LORAMAC_REGION_US915) || (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AU915)
|| (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AS923))
{
AppData.Buffer[i++] = 0;
AppData.Buffer[i++] = 0;
AppData.Buffer[i++] = 0;
AppData.Buffer[i++] = 0;
}
else
{
latitude = sensor_data.latitude;
longitude = sensor_data.longitude;
AppData.Buffer[i++] = GetBatteryLevel(); /* 1 (very low) to 254 (fully charged) */
AppData.Buffer[i++] = (uint8_t)((latitude >> 16) & 0xFF);
AppData.Buffer[i++] = (uint8_t)((latitude >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(latitude & 0xFF);
AppData.Buffer[i++] = (uint8_t)((longitude >> 16) & 0xFF);
AppData.Buffer[i++] = (uint8_t)((longitude >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(longitude & 0xFF);
AppData.Buffer[i++] = (uint8_t)((altitudeGps >> 8) & 0xFF);
AppData.Buffer[i++] = (uint8_t)(altitudeGps & 0xFF);
}
AppData.BufferSize = i;
#endif /* CAYENNE_LPP */
if (LORAMAC_HANDLER_SUCCESS == LmHandlerSend(&AppData, LORAWAN_DEFAULT_CONFIRMED_MSG_STATE, &nextTxIn, false))
{
APP_LOG(TS_ON, VLEVEL_L, "SEND REQUEST\r\n");
}
else if (nextTxIn > 0)
{
APP_LOG(TS_ON, VLEVEL_L, "Next Tx in : ~%d second(s)\r\n", (nextTxIn / 1000));
}
}
hi, my Get_temperature function always reads 0 if i tried to implement the sensor code in lorawan package.
can any one tell me what was the issue with the code. Im transmitting data in cayenne format
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.