STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WLE5 LoRaWAN --- code hangs in RTC module??

Good morning....Please refer to attached pics below:I have referenced Lorawan end node code from STM32 library for the STM32WL55 to use with my custom pcb that has an STM32WLE5.  The RTC section of the code is identical to that in the reference code....

SWenn1_0-1699279477692.png
SWenn.1 by Senior III
  • 1773 Views
  • 1 replies
  • 0 kudos

STM32WB55 LPUART Baudrate

Hi,I configured LPUART with 57600 baudrate. With this baudrate configuration Rx interrupt stop working if I send more than 11 bytes of Data on UART. With the same configuration there is no issue in transmit. Also in receive if I send less than 10 byt...

Sjain by Associate III
  • 4398 Views
  • 6 replies
  • 0 kudos

LoRaWAN CubeIDE configuration under LoRaWAN Middleware tab?

I have a custom pcb using a Seeed WIO-E5 module.  I found a github repo that supports the WIO-E5.  After downloading it and loading it onto my custom pcb my node joins the network and seems to work.  I notice however that the setting in the .ioc file...

SWenn1_0-1698933755201.png
SWenn.1 by Senior III
  • 1679 Views
  • 0 replies
  • 0 kudos

Resolved! Zigbee example/help on how to configure and send values ?

Hi all.I have been working with STM32WB for over a year and now starting up to use zigbee.Been trying the examples and digging deep into the internet on how to send values from a STM32WB that acts an temperature sensor. Not much info on ST & zigbee.I...

Lizerd_ by Associate II
  • 5846 Views
  • 4 replies
  • 0 kudos

STM32WB55RG - BLE DOESN'T WORK ON NEW STM32 PROJECT

Hi , I am working with STM32WB55RG-NUCLEO board. I've managed to upload the BLE_Stack_Full_FW and then when I try the example codes for BLE on my board, I can see the BLE advertising on my ST BLE ToolBox.However, when I try to follow the ST's youtube...

rehxes by Associate
  • 1728 Views
  • 1 replies
  • 0 kudos

STM32WL55 can't change FSK Data rate.

I use the wl55 on the nucleo kit, with the ping pong exemple (one core but same with 2) in subghz_phy_app.h i change the define for  #elif (( USE_MODEM_LORA == 0 ) && ( USE_MODEM_FSK == 1 ))#define FSK_FDEV                                   10000    ...

Xynium by Associate III
  • 2364 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.