2023-11-06 6:35 AM
Sometimes, if in addition to Bluetooth, WIFI is needed in the development of a product, the third module is used. Does ST plan to include WIFI in the e.g STM32W series in the future?
2023-11-06 7:18 AM - edited 2023-11-06 10:08 PM
Hello @Slh and welcome to the ST Community :smiling_face_with_smiling_eyes:.
At the moment, we don't have such a series. If you are looking for an ST Board that give you the opportunity to work with both Wi-Fi and Bluetooth. I suggest you use the B-U585I-IOT02A Discovery kit wish would provide Wi-Fi and Bluetooth communication and other interfaces that may help you.
Best Regards.
STTwo-32.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-06
6:46 PM
- last edited on
2023-11-07
5:05 AM
by
Lina_DABASINSKA
The author specifically asked about an integrated Wi-Fi, not a separate 3rd party module. Yet you are recommending exactly a 3rd party module. The real answer, which you should have given, is:
2023-11-07 1:29 AM
Thanks @STTwo-32 for your answer.
As "Piranha" pointed out, my question was about ST's plan to integrate WiFi and Bluetooth, so not using a 3rd module.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.