NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,are there any STM32 MCUs that support WiFi?The ST products I found on the internet are old and not recommend for new designs.I have attended a few STM32 security web events and find the security extensions of the current STM32WB series looks ve...
Hello,I'm trying to update the STM32WB15CC application with the ST BLE ToolBox.On the STM32WB15CC, the BLE_ota application is running (from STM32Cube_FW_WB_V1.17.0\Projects\NUCLEO-WB15CC\Applications\BLE\BLE_Ota).Connection with the STM32WB15CC is ok...
Has anyone out there done OTA with the WB1M? Did you write your own OTA bootloader from scratch, modify the WB55 Nucleo example from CubeWB, or some combination of the two? Any tips?I started trying to modify the example but I think the low level stu...
The following function aci_gap_update_adv_data returns the error 0x91 which means "Failed". We don't understand why we have this error and the startup of the device. Do you have any idea ?Best regards,Audrey
Hi, I made my first steps in ZigBee by using the NUCLEO-STM32WB55 board with the USB dongle. The dongle is flashed and the blue LED is shining, but the NUCLEO board is printing the following message: [M4 APPLICATION] ZbStartup Callback (status ...
Hello, This has happened before (here) and was fixed, but it seems that it is happening again.When the downloaded .zip file is opened with a text editor, the contents is:"Service unavailable, please try again later"Please can someone take a look at t...
I did not find a real UserManual for STM32WB55, with the register-definitions, peripheral explanations etc.?
Hi,is there an error in the datasheet? The data seems counterintuitive:FT pin input leakage current (max.) is- 150 nA for 0 to VDD-2500 nA for VDD to VDD+1V-250 nA for VDD+1V to 5,5VShouldn´t the last value be in uA perhaps?Kind regardsRené
Looking for CAD resources of NUCLEO-WBA52CG board. I couldn't find any of the CAD files for the STM32WBA chips. Please guide me in this... I have the NUCLEO-WBA52CG board but It will be useful for me if I have CAD files of the Board.
Hello,i am trying to get reporting from a remote temperature sensor Server ( End device) is use ZbZclAttrReportConfigReq to acheive it. I got a STATUS SUCCES in the callback but the device never send its temperature. Can you tell me if i miss sometin...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.