NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I use STM32WB05KZ. Could you give me an example about how to store configuration data to NVM by aci_hal_write_config_data() function? - When I tried to store to 0x00 (I used static randow MAC address), it returns 0 but the data is lost when th...
I want to add a EXTI0 line to act as a wakeup. I took the BLE_Heartrate example as a base. Out tyhe box, it compiles & runs ok. When I use CubeMX 6.16 to edit the BLE_Heartrate ioc to add PE0 as the EXTI0, next time I compile, I get an error that I'm...
I am using two Nucleo-STM32WL33 board, one as a transmitter and one as a receiver. The transmitter sends two messages in ASK modulation and the receiver records the messages in IQ sampling mode.Below is a visualization of the IQ samples time series.T...
Hello, I am currently working on a ble project on the stm32wb09ke nucleo board that uses the stm32 sequencer. My application is working as intended but I want to make it low power for optimal battery life. If i understand correctly the sequencer itse...
Hi all,I am currently working on the design of a custom LoRa/LoRaWAN-based IoT node using the STM32WLE5JCI6TR (bare MCU, not a module), and I am looking for a complete and reliable hardware reference design to follow.So far, I have identified the fol...
Hi all. Let me tell you the problem I'm facing and I googled for finding some help but without luck. The problem I have in hands is as next. I was using Nucleo WB55 to use the STM32F103CBT6 to program a microcontroller I have in a custom PCB for an e...
I am experiencing difficulty getting the NUCLEO-WL55JC1 to properly enter Shutdown mode. In some cases, the device appears to enter Shutdown mode but exits immediately. In other cases, it remains in Shutdown mode, but the current consumption is appro...
Hello everyone!I’ve been struggling to create a working application on the P-NUCLEO-WB55. My goal is to implement a Zigbee On/Off Client Sleepy End Device (SED) with NVM support, using buttons for control.I was able to successfully reproduce the On/O...
I have established BLE advertisement and connection is established successfully between ST BLE toolbox and the stm32wb55 based board. I am unable to read the chateristic value from the st ble tool box. My code is in custom_app.c file I2C_HandleTyp...
Hi! Starting a design with an STM32WL31K8V6. This is the 32 pin VFQFPN32 variant.As far as I can see, there is no HW Reference PCB that covers the 32 pin package. Looking at the datasheethttps://www.st.com/resource/en/datasheet/stm32wl31kb.pdfon p.32...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.