STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 300 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4117 Views
  • 0 replies
  • 3 kudos

STM32WB05KZ ADC Battery monitoring

I am using a STM32WB05KZ of a custom PDB, and I can not read a correct value of Vbattery.I have programed the ACD (+DMA) usgin CubeMX.   I use DMA to read the analog inputs:ADC_Conv_Cplt = 0; HAL_ADC_Start_DMA(&hadc1, value, 3); uint32_t start = HAL_...

Captura de pantalla 2026-03-13 100030.jpg Captura de pantalla 2026-03-13 100106.jpg
Ruben_EMI by Associate II
  • 772 Views
  • 10 replies
  • 0 kudos

Resolved! ST SDK for MuRata LBAA0QB1SJ-TEMP-EVK?

Hi, will ST extend I-CUBE-LRWAN support to include the new MuRata LBAA0QB1SJ-TEMP-EVK? Or offer a ST board based on LBAA0QB1SJ-295? Any suggestion on how to reconfigure the current I-CUBE-LRWAN version to work on the new EVK? We were previously using...

CCP by Associate III
  • 323 Views
  • 3 replies
  • 2 kudos

Resolved! STM32WB55; USB OutReport; not recieving data

Hello, I've been trying to setup bi-directional communication with USB-HID on a custom board with STM32WB55CEU. I can send data to the PC from the STM just fine. My usb stack runs, enumerates and reports correctly. However, when trying to send Data f...

Resolved! Lorawan end node - possible deveui bug?

I am trying to develop a small scale lorawan app on a nucleo-wl55jc using the application example in stm32cube_fw_wl_v1.5.0 and have spent several hours trying to trace my error/bug in the software. All join attempts fail because the deveui as it app...

jonnieh by Associate
  • 358 Views
  • 2 replies
  • 0 kudos

RAK3172 and UART 2 along with SUBGHZ

Greetings Everybody, Since few months i have been trying my hands on RAK3172. I have successfully implemented ADC, UART/USART and I2C on RAK but without SUBGHZ and everything is working fine. I have also made my custom code for RAK3172 SUBGHZ and it ...

BLE Thread dynamic stack broken in Cube v. 1.24?

After a long time, i started to look into using the BLE_Thread_dynamic stack image on WB55 again. First without success with my own code on my own board, which I do think to remember worked before.But afterwards with the BLE_Thread_dyn example on a W...

image.png Clipboard01.jpg
OliM by Senior II
  • 284 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.