2026-03-30 5:00 AM
Hi all,
I am currently working on the design of a custom LoRa/LoRaWAN-based IoT node using the STM32WLE5JCI6TR (bare MCU, not a module), and I am looking for a complete and reliable hardware reference design to follow.
So far, I have identified the following:
NUCLEO-WL55JC reference design files (schematics and PCB) from ST, which appear to be the closest official reference (even though it is based on WL55 dual-core variant)
Wio-E5 Dev Board from Seeed Studio, which is based on a module and does not expose the RF design details
While these are helpful, I am specifically looking for:
A reference design based directly on STM32WLE5JC (or very close variant)
Complete design files including:
Full schematics
PCB layout files
RF matching network implementation
Antenna routing
PCB stack-up / layer information
Since RF design (matching, impedance control, grounding, etc.) is quite sensitive, having a proven reference is critical.
Additionally, I would like to know:
:backhand_index_pointing_right: Are there any open-source or freely available reference designs based on STM32WLE5JC that include full PCB and RF layout details?
Any guidance, shared designs, or recommendations would be greatly appreciated.
Thanks in advance!
Solved! Go to Solution.
2026-03-30 6:03 AM
Hello @Vimukthi-Wathudura and Welcome to the Community,
Please refer to the following resources:
STM32WL5x-Ex wireless MCU lines - Wireless MCUs System-on-Chip Long-range communications
Data brief - STDES-WL5xxxxx - Reference designs for STM32WL5x and STM32WLEx microcontrollers
2026-03-30 6:03 AM
Hello @Vimukthi-Wathudura and Welcome to the Community,
Please refer to the following resources:
STM32WL5x-Ex wireless MCU lines - Wireless MCUs System-on-Chip Long-range communications
Data brief - STDES-WL5xxxxx - Reference designs for STM32WL5x and STM32WLEx microcontrollers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.