NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am working with the NUCLEO-WBA55CG board on a Zigbee_OnOff project, and I am facing an issue with the LED behavior.EnvironmentBoard: NUCLEO-WBA55CGMCU: STM32WBA55CGSTM32CubeMX version: 6.17.0Firmware package: STM32CubeWBAApplication type: Zigbee On...
Hi : I’ve been working on planning an STM32WBA25 series product recently. Regarding the antenna design, I’ve been referencing ST’s development board “NUCLEO-WBA25CE1.” From the MCU pin, the signal goes through an IPD, then a matching network, and fi...
Hi,UID is set at factory for all products? Wholesale ICs comes already programmed? I need to repair some machines and IC needs to have same UID as replaced. Thanks
Hi all,I recently designed and built a custom PCB for data acquisition and transmission through bluetooth using an STM32U575 as the main MCU and a BlueNRG-M2SA module for bluetooth data transmission configured as a Network Coprocessor. They are conne...
Hello ST Community,I am facing a critical issue with my STEVAL-PROTEUS1 board. The device is in a state where neither the wireless stack nor the application code can be updated or debugged.1. Corrupted Device Information (SWD_READ_FUS.PNG)When readin...
Hello,I am trying to setup the BLE stack on my custom board without LSE using a STM32WB55CEU6. I have multiple boards on hand, on the first one, appe_Tl_init(); worked fine and I got to the BLE stack initialization code. However BLE never worked due ...
I have question on STM32WBA65RI uC we are using it for our products TEK923/926. It seem to me that BLE stack doesn’t allow to use Free Running Binary mode and Calendar Mode.There is option of MIX Mode in CubeMX but doesn’t seem working. Causing not t...
My BLE project on stm32wba65 makes use of "UTIL_TIMER_Create" to set a callback. This works ok when the RTC is configured just as free running binary. If I set the rtc mode to mixed binary & bcd, the callback never gets fired. I'm using an LSE to dri...
Hello,I am using NUCLEO-WB05KN1 development board with the embedded STM32WB05KN MCU.My goal is to advertise in Eddystone UID frame format.Currently I generate the advertising packet manually and insert:10-byte Namespace ID6-byte Instance IDAdvertisi...
I have a STM32WB55 board where I have two I2C connections:1. LSM6DSO IMU2. TCA9548A with downstream I2C to hall sensors The TCA9548A I2C multiplexer does not ACK when addressed. The firmware scans 0x70 (this should be correct already)–0x77 and gets n...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.