NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello. We are developing a p2p application using two Wio-E5 mini modules based on stm32 WLE5JC.The problem I'm facing is HAL_DELAY not working. I created the project, chose HSE, LSE, then SysTick, and then after I selected SysTick, HAL_IncTick() was ...
I want to disable the AGC and use supply manual attenuation values.Disabling the AGC is pretty straight forward, I just set the AGC_EN bit in AGC0CTRL to zero.This works fine, but the gain/attenuation is fixed at the reset value and I'd like to use a...
Hi together, I have been developping a simple BLE application (that I can attach eventually) on the STM32WB55RG P-Nucleo This application combines BLE + USB Device (FS) But after I upgraded the BLE stack firmware from: FUSVER:1.2.0.0STKVER:1.13.2.2ST...
The STM32WB55 it will jump to the SysTick_Handler interrupt handler routine after we have configured the clocks and the RTC and then enable the interrupts. I don't understand why this is happening. I have checked the following registers:SysTick->CTRL...
Hello, I am using different ST MCUs from few years and already have a wide set of development boards, tools and JTAG emulators and so far did not experienced any troubles to attach new board (even custom made) to CuveIDE and to flash and debug my sol...
hello everyone, i am a beginner in STM32cube. i was working on board Nucleo wb55rg. and following this tutorial STM32WB Getting Started Series: Part 12a, STM32CubeMX & STM32CubeIDE lab. Introduction, and it said on 2:33 that i need to activate "syste...
HiIf I develop an application using the STM32WBA25 MCU with BLE, ThreadX, and USBX, is the RAM size sufficient?
Hello everyone!I am trying to get all services and characteristics from steval-stwinbx1 board running FP-SNS-Datalog2 function pack. Here's simple program I wrote:import asyncio from bleak import BleakClient MAC_ADDRESS = "DA:3E:83:DD:30:F8" async ...
Hi everyone, I am working on a Beacon project using NUCLEO-WB05KN. My goal is to broadcast Eddystone-UID and allow a connected phone to update the Namespace ID and Instance ID via GATT characteristics. The Setup: I have a Custom Service with two cha...
Hello, I'm using 2x NUCLEO-WB55RG boards with the unmodified BLE_MeshLightingPRFNode example from STM32CubeWB V1.24.0. Setup:- BLE Stack full v1.13.2.2 (stm32wb5x_BLE_Stack_full_fw.bin)- FUS v1.2.0- Provisioned with ST BLE Mesh app (tested on both iO...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.