NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
1. Requirement description It is expected that the terminal can join the network with the specified panid 2. Problems encountered during the test 2.1 It was found that the given function ZbStartup cannot enable the terminal to join the network with t...
Dear sir / madam The UltraLibrarian WBA5M (Module) footprint is flawed. Potentially it can screw the module under reflow.Those center GND pads are not placed correct. I noticed when comparing the ST dev-board module. see image..
Hello,I am having some hard time to connect my nucleo-wl55jc1 to any LNS, even though i checked that Device, Join, and App EUIs are all correct and there is no mismatch, but whichever LNS I try, I always get the same result First, I tried with an ind...
I have been working with the single core LoRaWAN_End_Node example application on a B-WL5M-SUBG1 board with good success. With STM32CubeMx v6.16.0, WL Firmware 1.4.0, I see a current draw of under 2uA between transmissions.Last week I upgraded STM32C...
Hello, I am currently developing a project that requires an ultra-low-power BLE-based indoor localization tag. The device should periodically wake up and advertise, remaining in standby mode (targeting approximately 500 nA to 1 µA) for about 90% of...
Hello,I am currently working with the NUCLEO-STM32WBA65RI. My main goal is to place the board in Standby mode and periodically wake it up to perform BLE advertising (as a Peripheral), while still allowing it to handle a possible connection request f...
Hello, I am currently working with the NUCLEO-WB05KN1 development board (STM32WB05KN MCU) and I would like to implement FOTA (Firmware Over-The-Air) / OTA update over Bluetooth. However, I could not find any clear reference documentation, application...
Title edited to clarify that this refers to a NUCLEO-WBA65RI board.Hello, I am currently using STM32WBA65RI with Standby mode. According to datasheet, this mode should be able to reach 120nA current consumption with the 16 GPIO wake-up pins (RTC disa...
Hi, I am using STM32WBA55G-DK1 as a BLE TMAP Peripheral, I have a transmitter, which is transmitting 4 channels/subgroups of data. But the device is stucking at Syncing PA, but when the same is given with 2 channels(BIS), I am able to to connect and...
I am working with the STM32WB5MMG and implementing firmware updates using OTA. For testing, I am using the ST BLE Sensor Android application. What I Tested I first tested OTA using the example projects available in the STM32CubeWB firmware package: ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.