STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

toughgfx change screen from button virtual function?

Hi all,I want to change from firstScreen to secondScreen if there is some text displayed on the firstScreen. I found an old post (here) where the accepted answer says it is difficult right now and working on a better way ... that post is from 2019 th...

Rodo by Senior
  • 2272 Views
  • 2 replies
  • 1 kudos

Resolved! Re: STM32F769I-DISCO - Really noisy TFT LCD display

Hi everyonei worked fine with MB116-A03 display and now i have the same problem with A09 display. I made the changes available on github:- created the new component nt35510 with the three files (.h .c .html)- and made changes to 4 files: stm32f769i_d...

MikParà by Associate
  • 2084 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX and Textarea problem

HelloThis problem has arised when creating a more complex program and I have narrow it down to a single test.project. I have created the usual project for the STM32F769 Disco using TouchGFX 4.20 Designer . I have set only one single TextArea, configu...

jtpgilej by Associate II
  • 4075 Views
  • 4 replies
  • 0 kudos

Urdu language

Hello community,I'm currently working on a project that requires using the URDU language with TouchGFX. Unfortunately, there seems to be no native support for URDU in TouchGFX according to the documentation. I was wondering if anyone has come across ...

DanielAb by Associate
  • 1521 Views
  • 1 replies
  • 0 kudos

Resolved! Wrong position of a "." on a Button with Label

The position of the text containing only a dot on a Button with Label is wrong. Left picture is a screenshot from TouchGFX Designer, where the dot is well aligned. To the right a framebuffer-screenshot of the actual application running on target hard...

Dot in the Designer.png 2023-07-10 15-06-04 Screenshot.bmp
t.decker by Senior II
  • 1919 Views
  • 2 replies
  • 2 kudos

Mikroe Fusion V8 - Touch Interface

Hi all,Lately I purchased the FusionV8 board by Mikroe to play around with. Currently I have a STM32F407ZG mounted on it, but I can change it with a douzens of other STM's. Also included a 7 inch tft capacitive board to do some testing with.I was won...

jdammerz by Associate
  • 1189 Views
  • 0 replies
  • 0 kudos

Resolved! Can not convert my project to TouchGFX 4.22.0

Hello ST Team,I have a huge TouchGFX project (80+ Screens, several Containers,  400+ images), which I am currently working at using version 4.21.4 (generated with Cube V. 6.8.0). This version is working perfectly. I can generate code, add screens and...

GS1 by Senior III
  • 2577 Views
  • 3 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.