STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32 VS Code Extenstion with TouchGFX

Hi,I'm having an issue building TouchGFX project in new VSCode extenstion. When building cmake is throwing an error:cannot find -ltouchgfx-float-abi-hard: No such file or directory.Project is builiding and compiling in STM32CubeIDE just fine.

xmisgu by Associate II
  • 2352 Views
  • 1 replies
  • 1 kudos

Unicodechar to char

How to change type from Unicodechar to char? I'm trying to pass char to model like this, but it only passes one character. What I am doing wrong?  

heyo_0-1689660758663.png
heyo by Senior
  • 2529 Views
  • 2 replies
  • 3 kudos

SDRAM MPU configuration

I store "FrontendHeap" to my external SDRAM and in the text appears question mark and when I want to change screen it crashes at specific screen.I configured my SDRAM   void MX_FMC_Init(void) { /* USER CODE BEGIN FMC_Init 0 */ /* USER CODE END F...

Photo 2023-08-02 10 27 44-min.jpg
heyo by Senior
  • 3262 Views
  • 4 replies
  • 0 kudos

TouchGfx custom container

Is there any way to update 4 textarea with a single invalidate call? Or is there any way to add multiple text area in a custom container and update all text area with a single call of invalidate?

spate.2 by Associate III
  • 5292 Views
  • 6 replies
  • 0 kudos

TouchGFX Arm Cortex-M3 support

I know, there are a lot of posts about this topic. But I am curious that there is any new improvement.I am working on the STM32F207 series MCU. I built the code by using the core library for Cortex-M0. But I don't know that it will work or not. Did a...

hsynk by Associate II
  • 1107 Views
  • 0 replies
  • 0 kudos

Resolved! Changing Font properties on run time in TouchGFX

I have a list of Menu items. I'm handling the navigation with buttons. When curser/pointer pointed on a particular menu Item, The existing text should look darker than other items. Example (Sorry about the poor outline :grinning_face_with_sweat:). Se...

Manu1_0-1690804183604.png
Manu1 by Associate
  • 1672 Views
  • 1 replies
  • 0 kudos

STM32H750 LCD flickering

Hello,I am working on a custom board with STM32H750XBH6 MCU.In my project I am time to time getting LCD flickering issues. First it was only visible in release version. Then after switching off the compiler optimizations, it worked. Again I have got ...

Dinushka by Associate II
  • 4033 Views
  • 5 replies
  • 1 kudos

Screen to screen data transfer

Hi,I wanted one data that I received from back end to be displayed in both in startup screen and screen2 which comes up after startup screen.So once I receive the data from back end in startup screen via Model.cpp I have to save it in Model.cpp and w...

KNara.2 by Associate III
  • 1362 Views
  • 1 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.