2023-08-03 10:54 AM
Hi all,
I'm making my project and adding screens and stuff and I noticed that if I add an interaction to a button as a virtual function, and add a function name, the function does not get automatically added to the code in the *.hpp and *.cpp files for that screen. I end up having to go back and forth between the designer and cubeIDE to copy/past the function names to the files. I had like 15 functions to add. Am I missing a setting somewhere to autogenerate the virtual function names in the files or it is suppose to be manually done?
Thanks
2023-08-03 11:16 AM
Hello
Ready declarations can be found on the view class base .hpp- file under gui_generated folder (for example Screen1ViewBase.hpp).
It is bit easier to copy those there to view class hpp / cpp.
Br J.T
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.