2023-06-23 6:00 AM
Hello ST Team,
I have a huge TouchGFX project (80+ Screens, several Containers, 400+ images), which I am currently working at using version 4.21.4 (generated with Cube V. 6.8.0). This version is working perfectly. I can generate code, add screens and so on. As this is not yet a released project, I thought it would be good to convert it to the latest version 4.22.0. However this fails to load the project at all. The designer simply closes after 2 minutes (when the project would normally appear) without any comment or other error message.
I can not send the project to you as it is confidential and furthermore it is not a standalone project. There is a second CPU involved. It is a custom board with LCD 480x800.
How can I help to find the reason for this crash ?
Best regards
GS
Solved! Go to Solution.
2023-06-26 1:17 AM
2023-06-26 12:23 AM
Hello @GS1,
Could you share the .log file of TouchGFXDesigner ?
You can find it here : C:\Users\username\AppData\Roaming\TouchGFX-4.22.0\.
Thanks for the report !
2023-06-26 1:17 AM
2023-08-02 7:32 AM
Hi Osman,
I have the same problem changing my project from 4.20 to 4.22, because I am also interested in the new image compression. It would be great to get an information when this bug is fixed or a workaround is known.
Thanks for a while.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.