STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is DMA circular mode and in ADC DMA continuous request

Hello ! [STM32L073RZ]I've been thinking what is this ADC DMA continuous request. I don't really much know what it is exactly and why it must be enabled. I know there are 2 modes of DMA, which is normal and circular in which normal starts only once an...

Xenon02 by Senior
  • 12358 Views
  • 8 replies
  • 1 kudos

Resolved! STM32F070RBT using PLL with HSI RC

Evaluating the STM32F070RBT6 for a project, and using STM32CubeMX V6.10 I am unable to connect the PLL to the HSI RC. It all works ok if I use HSE.I'm wondering what I'm doing wrong. 

CWedg.1 by Associate III
  • 2349 Views
  • 2 replies
  • 0 kudos

Combining bootloader and application code binary file

Hi, For our project we have one Bootloader in 0X80000000 and application program in 0X80001c00. We have to combine both of these binary files and load it in to our controller. What is the best way to combine two binaries ? We are using windows platfo...

Deepu joy by Associate II
  • 1475 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U575: VDD 1.8V and USBVDD 3.3V - FAILs (no USB)

I want  to run MCU with VDD 1.8V (in order to have all I/O-signals as 1.8V). I changed to use a LQFP64 package which provides a dedicated pin for VDDUSB.I power VDDUSB with 3.3V (for sure not below 2.7V) but all other VDDs on MCU are 1.8V:USB functio...

tjaekel by Lead
  • 5462 Views
  • 2 replies
  • 0 kudos

SMT32F042K6T7 temperature issue

Hello, I am using STM32F042K6T7 microcontroller for doing some start-up configuration for some Ethernet PHYs by SMI, it is working well at room temperature, and cold (-40°C), but when I increase temperature max (+74°C) the microcontroller it seems is...

ArturIn90 by Associate II
  • 2650 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H747I-DISCO Virtual Com via USART to arduino

if I configure the USART and use HAL_UART_Transmit. The UART to USB bridge is taken care of by the ST-Link chip.Could i use the VCP on the board is on PA9/PA10(pin D14 and pin D15 to rx and tx to arduino) and use digital.read on arduino to get the in...

wjian2_0-1690904059020.png
wjian.2 by Associate III
  • 3409 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H747IX SystemClock_Config problem

I have configured the M7 clock to 480 MHz and the M4 clock to 240 MHz using the HSI as input.  In SystemClock_Config routine the statement__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);is crashing the STLINK-V3 with the error messageEr...

Olivili by Associate II
  • 1602 Views
  • 2 replies
  • 2 kudos

Resolved! BKPSRAM corrupted after power cicle

Hello,I'm using a STM32U5A5VJTXQ MCU and I need to use the 2K BKPSRAM located @0x40036400.I can read and write without problem the BKPSRAM after power up, but a power cycle corrupt all the content. Strangely, the RTC content: time and registers, are ...

clemente by Associate III
  • 3746 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.