2024-01-17 2:35 PM
I have configured the M7 clock to 480 MHz and the M4 clock to 240 MHz using the HSI as input. In SystemClock_Config routine the statement
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
is crashing the STLINK-V3 with the error message
Error in executing 'step' command ...
Target is not responding, retrying...
I had a breakpoint at that line and activated it with the Step Into (F5).
Solved! Go to Solution.
2024-01-17 2:40 PM
First set speed lower....and see ds, whats max.:
Maybe: set at 200M + 100M , then go on. CubeMX should show you allowed speed vs scale and wait states.
2024-01-17 2:40 PM
First set speed lower....and see ds, whats max.:
Maybe: set at 200M + 100M , then go on. CubeMX should show you allowed speed vs scale and wait states.
2024-01-17 2:50 PM
Brilliant. That solved my problem. Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.