STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Erase - unlock STM32L083

I am using STM32L083 and need to erase it using J-Link. If it is locked at Level1, I also need to unlock it. My goal is to completely erase the entire Flash memory. I believe I have an error in the process, as I have been unsuccessful in both erasing...

JR2963 by Senior II
  • 2148 Views
  • 0 replies
  • 0 kudos

Resolved! Can the STM32H7x M4 core boot from SDRAM or not ?

According to the STM32H7's datasheet, the M4 core shouldn't be able to boot from an SDRAM memory address (because it's outside of the range 0x00000000 to 0x3FFF0000):However, I found out that I can actually boot the M4 core from SDRAM, if I used the ...

IbrahimAbdalkader_0-1705573213089.png

Resolved! STM32C011J4M6 conflict on pin

Hello everyone,I have a question about the STM32C011J4M6 in S08N package.I am developping a PCB with this MCU and want to use an LSE like in the picture below.Then I also want to program and debug my MCU with an stlinkv3 and will use the SWD debug so...

Pierre75_0-1705586401952.png Pierre75_1-1705586566297.png
Pierre75 by Associate II
  • 4664 Views
  • 6 replies
  • 0 kudos

Can the STM32G030 nRST pin disabled, or be used as GPIO?

Hi guys!We are running a project using STM32G0 MCU-s. We used STM32G031 in the previous iteration, but, due to budget reasons, we now ended up with STM32G030-s, beleiving these are basically interchangeable for our purposes. Due to some board error, ...

TLaut.1 by Associate
  • 10599 Views
  • 10 replies
  • 2 kudos

Resolved! STM32 GPIO pin small output voltage

Hi,I am switching PB12 on/off with 1 second delay on STM32F030C8T6. Measuring with the multimeter, the HIGH state is only 0.2 volts, even though Vdd is 3.3V. I have turned off all things that could be drawing too much power from the MCU. Other pins o...

JS8 by Senior
  • 5343 Views
  • 4 replies
  • 2 kudos

Timer 1 output pin not performing PWM

I have defined PE9 as belonging to Timer 1;I setup timer 1 as PWM as shown above.When I enable the timer, nothing happens at PE9.I tried setting force  high; no changeWhen I define PE9 as standard output forced high, it goes high.  So I know that the...

Leroy3_0-1704906464221.png
Leroy3 by Associate II
  • 2834 Views
  • 4 replies
  • 2 kudos

Why led isn't blinking when i press the button?

I am tring to write a code for stm32f401cb which will blink the led when i press the led and when i leave pressing the button,it will turn out the led.I have set channel ahb1 which connects to port a and b in my microprocessor f401cb and i chose inpu...

hold button.PNG
YagciOnur by Associate II
  • 2816 Views
  • 3 replies
  • 0 kudos

How to start PWM using the registers.

What am I doing wrong?Why is PWM don't work on the STM32F767ZI? RCC->APB2ENR |= 1; // Enable clock for TIM1 on APB2. RCC->AHB1ENR |= RCC_AHB1ENR_GPIOEEN; // Enable clock for GPIOE port on AHB1. GPIOE->MODER &= ~(1 << 18); // Clear/reset PE9 mode. GP...

Q1.png Q2.png Q3.png
DK.7 by Senior
  • 7234 Views
  • 13 replies
  • 2 kudos

About H563 IAP

Used nucleo-h563zi board.Below is bootloader jump.Below is app. question:I first download app through CubeIde,this code is run success,and every function is OK.But i reset this board,the code will enter NMI interrupt. 

Sunwaz_0-1705568171944.png Sunwaz_1-1705568203111.png
Sunwaz by Associate III
  • 1473 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.