STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! high speed fdcan stm32g431

Hi, i'm dealing with fdcan and have problems with high speeds, 1Mbps works good, but 8Mbps (which works in loopback mode) doesn't, I tried with delay compensation, but didn't work, or maybe i used it wrong way? static void MX_FDCAN1_Init(void){ /* US...

Tomuello_0-1707842474878.png
Tomuello by Associate II
  • 3063 Views
  • 3 replies
  • 0 kudos

STM32H747XI OTA

Hi,I will be using STM32H747XI with a MIPI or RGB-24bit display and design screens using touchGFX. My question is does it support OTA  via QSPI flash storage as the Arduino framework has support for the OTA does the Cube IDE support it or can I use A...

Basit009 by Associate
  • 889 Views
  • 0 replies
  • 0 kudos

Resolved! CAN bus doesn't work in loopback mode

  Hi I followed this yt-guide for CAN-bus https://www.youtube.com/watch?v=JfWlIY0zAIc&t=918s I'm however using a different type of nucleo board (L433RC-P in my case and F103C8tx in the video) and a different type of CAN-transceiver (MCP2561T-E/SN vs...

Mr4_0-1707733361123.png Mr4_1-1707733423132.png Mr4_2-1707733462396.png Mr4_3-1707733661815.png
Mr4 by Associate III
  • 10133 Views
  • 12 replies
  • 4 kudos

Resolved! OTP -Memory Location

hi,i couldn't chase which location address allotted for OTP memory ?.As per data sheet of MCU - Stm32f401ccu6– 512 bytes of OTP memory allotted . Can anyone please detail me OTP location Start Address - End Address 

MMARI.1 by Senior II
  • 2152 Views
  • 2 replies
  • 0 kudos

Resolved! What is VDDA_Charac on the STM32F072?

Apologies if I've missed something simple (and I probably have!), but I'm trying to convert ADC readings on the STM32F072 into actual millivolts and I cannot seem to put all the pieces together.Where I am currently stuck is the formula at the top of ...

BWKidd by Senior
  • 4058 Views
  • 4 replies
  • 1 kudos

Resolved! Using classical CAN with FDCAN controller on STM32H743VIT6

Hello. I have three question about using classical CAN frame with FDCAN controller.I am using STM32H743VIT6 MCU on my PCB. 1. If system clock(label in ioc file: SYSCLK) is too low, can it make impossible to use CANbus? 2. If I using only classical CA...

LSH by Associate II
  • 4760 Views
  • 3 replies
  • 1 kudos

Accidental EXTI-Interrupts on STM32H735

Hello,maybe someone has an idea or can share an similar experience. Since I'm currently in the evaluation phase for selecting an MCU for our new industrial embedded project. I want to inspect and analyze this problem, to be sure the used MCU is worki...

AZorn.1 by Associate III
  • 15474 Views
  • 30 replies
  • 10 kudos

Compilation error while integrating DSP library

While replicating the method of integrating DSP libraries into my STM32 project as discussed in the following thread: tutorial , I encountered the error #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" du...

error_fpu.png solucao.png resultado.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.