STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to connect the MIPI display with ST controller

Hi Team,We have an LCD with a MIPI display. We need to connect with the STM32 MCU.Please find the pin details on the LCD. We need to connect MIPI_0+, MIPI_1+, MIPI_2+, MIPI_3+, MIPI_4+,MIPI_0+, MIPI_1-,MIPI_2-, MIPI_3-, MIPI_4-.Kindly suggest ST cont...

SK22_0-1704367201554.png SK22_1-1704367266591.png
SK.22 by Associate II
  • 2932 Views
  • 4 replies
  • 1 kudos

COMP and blanking Function

Hi all,I am having some problems connecting a comparator to a TIMER using its blanking function (as described in the AN4232 application note).I've read the COMP_OutputBlanking example found in the STM32G4 repository projects (I'm using a STM32G431).I...

FlavioB by Associate II
  • 2171 Views
  • 2 replies
  • 0 kudos

Resolved! Pulses to KWh conversion in Energy meter

Hi,I am working with STM32G491RE.I communicating  ATM90E26 single phase energy meter with STM32 through SPI communication.I can able to read voltage ,current values correctly from the meter.For KWH calculation, I am reading Absolute active energy reg...

sireevenkat1_0-1712211776138.png

Resolved! FMC-SRAM Configuration for STM32F40G-EVAL

Hello there,   I am working on a project using an STM3240G-EVAL board which as the STM32407IGH6 MCU on it. In this project, I want to use USB-OTG-FS to connect an external USB microphone to the board and then store any information sent into the micro...

STM32H723ZG reading vref problem

Hello, i am trying to read internal temperature and vref values from ADC3. I shared ADC3 ioc settings. ADC clock mux freq is 96MHz and sampling time is set to ADC3_SAMPLETIME_247CYCLES_5.On init routine calibration line as below :HAL_ADCEx_Calibratio...

iocADc.PNG
Enes1 by Associate
  • 1007 Views
  • 0 replies
  • 0 kudos

Infrequently getting UNALIGNED HardFault

Hello There,I'm working on a FREERTOS based STM32H7A3 application.Upon debugging, my code randomly halts on UNALIGNED hardfault. The occurrence of this fault condition is very rare. During my testing in the last 30days, I ran into this for nearly 3 t...

KAgga1_0-1712212064993.png KAgga1_1-1712212107019.png KAgga1_2-1712212277969.png KAgga1_3-1712212424110.png
KAgga.1 by Associate III
  • 1924 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 IC's Unique ID

Hi,I am using STM32G491RE MCU for my project. Is it true each STM32 IC has its own unique ID. For STM32G4 product has the UID facility. Is it 96-bit ID for all the stm32 families or is it different.Which manual has to be referred for this?If yes can ...

[STM32h7] ADC3 BDMA Transfer error (Buffer located in SRAM4)

I understand the STM32H7's BDMA requires special attention to the memory map [FAQ: DMA is not working on STM32H7 devices]however, when I try to declare the buffer to SRAM4 that will be the destination for the ADC DMA transfer, __attribute__((at(0x380...

EZamo.1 by Associate III
  • 6231 Views
  • 6 replies
  • 0 kudos

Resolved! USB FS Support

I am working on OTG FS application on stm32f769 discovery board, as per the it's schematic for OTG_FS VBUS power supply will be taken care by External Phy(see below image). So as per that I configure the STMCUBE IDE, and i disabled the VBUS_Sensing a...

Shikamaru_0-1711460081875.png
Shikamaru by Associate III
  • 2813 Views
  • 4 replies
  • 1 kudos

STM32H563ZI LINKER

Hi,I am working on freertos plus tcp library with STM32H563ZI, but how must I make memory otions in linker file?like: RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320KFLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048KRAM1 (xrw) : ORIGIN = 0x20000000, LENG...

Recep by Associate II
  • 8678 Views
  • 11 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.