STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Switch off VREFBUF on STM32U5

Is it possible to switch  VREFBUF clock off after configuration for power save? So the clock is off and the buffer is providing Vref.In DS there is no mention about it (e.g OPAMP has this note).

STM32H5 SPI DMA LL Transfer Timing Issue

Hi All,I’m new to using the STM32H563 solution. To send SPI data using DMA, I referred to the sample code from the SPI DMA sample of the H533RE project.I'm not sure when exactly the SPI is start to transfer the data by DMA.The following is a part of ...

PeterTseng_0-1712884196104.png

Updating firmware via IO-Link

Hello,I have a question regarding doing a firmware update via the USART-pins and IO-Link.Would it be possible to use a IO-link master module to sent an update to the L6362A which translates it to 3.3V UART for the STM32G0B1KEU6 we are using in our cu...

GOjayson by Associate
  • 1087 Views
  • 0 replies
  • 0 kudos

STM32F401RCT6 requires a reset to run code

We have a new revision that has a significant population of boards with this intermittent power issue. steps to reproducepress power buttonpower applied to the MCU the MCU only prints a single debug message, then haltspress reset: device works normal...

OCTOSPI line idle level - Weird behaviour

Hi, Community,I'm trying to understand the OCTOSPI peripheral on my STM32L4P5. I'm new to STM32, but old in embedded. Particularly, I need to know/affect the idle level of the data line of the OCTOSPI. I thought that the last transmitted bit would re...

DS0002.png DS0001.png

STM32 Phase Vocoder Algorithm

Hi! I'm looking to implement a phase vocoder algorithm on an STM32F4/STM32F7 and I was wondering if anyone has already done this and can provide suitable resources?Thanks!

Resolved! UART TX and RX pin issue

Hello,I am using "NUCLEO-H743Zi2" eval board. I am using it for UART communication. I had configured UART4 in it as following;PA0 as UART4_TXPA1 as UART4_RXWhen I tried to transmit, it is not transmitting more than 2 bytes. While receiving, it is not...

adithya_sharma_0-1712761586212.png

I2C Slave Receive in DMA mode on STM32U575 series

Hi,I'm attempting to set up an STM32U575 as an I2C slave. (The master is a F301)My problem is that the slave only receives one byte, and then proceeds to disregard all of the following data.I have set up a switch that turns on an RGB LED, depending o...

Screenshot 2024-04-11 at 05.51.14.png Screenshot 2024-04-11 at 05.53.02.png Screenshot 2024-04-11 at 06.00.40.png Screenshot 2024-04-11 at 06.15.33.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.