cancel
Showing results for 
Search instead for 
Did you mean: 

Switch off VREFBUF on STM32U5

Tomas Hamouz
Associate III

Is it possible to switch  VREFBUF clock off after configuration for power save? So the clock is off and the buffer is providing Vref.

In DS there is no mention about it (e.g OPAMP has this note).

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MGAGE.1
ST Employee

Hello @Tomas Hamouz

Yes, it's possible to switch off the clock of VREFBUF for power save. 

Once the VREFBUF is configured and stabilized, the clock can be disabled, while the buffer continues to provide the reference voltage.

If you need to reconfigure VREFBUF, you will need to re-enable the clock, make the changes, wait for stabilization, and then disable the clock.

Thank you for your message, 

Best regards.

 

 

View solution in original post

1 REPLY 1
MGAGE.1
ST Employee

Hello @Tomas Hamouz

Yes, it's possible to switch off the clock of VREFBUF for power save. 

Once the VREFBUF is configured and stabilized, the clock can be disabled, while the buffer continues to provide the reference voltage.

If you need to reconfigure VREFBUF, you will need to re-enable the clock, make the changes, wait for stabilization, and then disable the clock.

Thank you for your message, 

Best regards.

 

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.