STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FreeRtos not all tasks are running

Hello, I have a problem with threads. All of them are of same priority, with osDelay(300), except the uartThread which has osDelay(1). Everything else is the same for all threads. I have allocated 20k of HEAP and in ioc file it says im using only 3.5...

PPopo1_0-1712832411372.png
PPopo.1 by Senior
  • 1959 Views
  • 1 replies
  • 0 kudos

EOCS( End of conversion selection) bit in ADC of STM32F401RE

Hello All,    I am trying to write a baremetal code for ADC, to work in Continous SCAN mode. I needed help with a few bit in internal ADC peripheral in STM32F401RE1. EOCS As per the RM, if EOCS is "1" then EOC is set for each conversion,hence suppose...

NNada1_0-1712838923124.png
NNada.1 by Associate II
  • 1841 Views
  • 0 replies
  • 0 kudos

Resolved! Multiplex 1 output to 12

Hello,What is the best way to multiplex an output pin to 12 output signals?  I currently have 1 output sourcing 3.3v through a 1k resistor which works well, but need it multiplexed to 12 identical outputs.  I see the STM32F373 has a max rating of 15m...

LMorr.3 by Senior II
  • 3471 Views
  • 9 replies
  • 8 kudos

Resolved! NUCLEO-U575ZI DMA->DAC doesn't work (USEF)

Hello everybody! I have a sine-wave array, that I throw to the DAC, triggering it by TIM6. When the TIM6 interrupt routine is responsible for supplying samples - everything works fine, but when I try to use DMA nothing works. The DMA keeps spitting t...

Skfir by Senior
  • 2239 Views
  • 2 replies
  • 0 kudos

usb communication

Hi, I want to make communication between stm32h563zit6(Nucleo-H563zi) via  USB communication, i have tried configuring various UART/USARTS but not able not make communication.I had verified it by sending some data from stm32  ,and tried to see it on ...

mahaveer by Associate
  • 1167 Views
  • 1 replies
  • 0 kudos

STM32F405芯片USART 2M波特率下DMA收发丢数据

我用板子A:STM32H743VIT6,HAL库开发,版本v1.9.0HSE=20M,主频480M串口1使能,DMA发送,IDLE+DMA接收数据。发送使用1ms定时器进行DMA串口发送,发送间隔1ms,发送数据长度18字节。板子B:STM32F405RGT6,HAL库开发,版本v1.27.0HSE=8M,主频168M串口2使能,DMA发送,IDLE+DMA接收数据。数据发送使用1ms定时器,10ms间隔通过DMA发送数据,发送数据长度18字节。连线板子A的Tx-板子B的Rx。板子A的Rx-板子...

loganm122 by Associate II
  • 3123 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.