STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32l431rct HardFault using spi, adc , RTOS

Hello im Khoi. i get big trouble with stm32l431rct, when i using freeRtos . Task1 i using spi comunication . Task2 i get ADC DMA . When i disable Task2 program no problem. But i enable task2 get problem spi hardfault-Handler . Excuse me :(( 

Resolved! bluetooth communication problem when working with two UARTs

Hi during development of program I found weird behaviour. I am using STM32G030C8T6 MCU. I am trying to connect external device using HC-05 bluetooth module. In my project I also connect with devices using MAX3485 module for RS485 communication. I wro...

MaciejG by Associate II
  • 2192 Views
  • 3 replies
  • 2 kudos

Ux_Device_HID for STM32U575ZI

Hello,I wonder if it exists an Ux_Device_HID example project for STM32U585ZITxQ mcu or the way to convert the Ux_Device_HID project for STM32U585AIIXQ present in the examples for a different packaged mcu. Best regardsIlaria

Ilaria by Associate
  • 1677 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO-F412ZG CAN Communication, No RX and No tx

I am using CAN1 pins to Connect to the driver board (SN65HVD230).      All Voltages are good. I am using 2 PCAN dongles with 120 Ohm terminations at both ends of the BUS with the Nucleo CAN shown above in the middle of the bus.  I ported the code f...

JDOG_3-1712698313675.png 0405241626~2.jpg JDOG_0-1712696721291.png JDOG_1-1712698012460.png
JDOG by Associate III
  • 3124 Views
  • 3 replies
  • 1 kudos

TCS peripheral

Hello,I have custom board with STM32F301R8T6 and connected 4 channel slider sensor. I want to copy an example present in STM32CubeIde called TouchSensing_Linear. There in the configuration files such as tls_user.c, tls_user.h are includes for tls.h a...

Resolved! STM32H74 ECC Errors

Hi,Some doubts on the ECC functionality on STm32h74x.How can we know if the data can be corrected for cases DEDF and DEBWDF ? I always see the DEDF and SEDF fields set in my case. This bits are set when the control is hit the main(), and then I clear...

andy_long_0-1712312892764.png andy_long_0-1712315036609.png andy_long_1-1712315066857.png
andy_long by Associate III
  • 5266 Views
  • 9 replies
  • 1 kudos

Resolved! Package data register wrong code

Hello,I am using a STM32G491 in LQFP48 package. In the RM0440 rev8 page 2122 the package code for LQFP48 is 01011. But I read 01001 which would be LQFP32. The device id 0x479 is correct. Is there a reason for this? Thanks.

Resolved! EEPROM emulation firmware library

I'm working with a legacy project that uses some EEPROM emulation code on a STM32F103 MCU. I need to find the original release file containing eeprom.c and eeprom.h of that emulation code. The description of the header file looks like this:  /*******...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.